Console stops after buildroot login

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Console stops after buildroot login

2,565件の閲覧回数
surajkumarmokha
Contributor I

Hello,

I am using imx6q sabrelite board with sd card booting with buildroot has my development tool.

I am able to boot till kernel and able to see buildroot login. But once password is provided. console stops responding.

Any suggestions where can be the issue.

Below is boot log :

U-Boot 2016.03 (Dec 06 2016 - 16:41:34 +0530)

CPU:   Freescale i.MX6Q rev1.2 at 792 MHz
Reset cause: POR
Board: SABRE Lite
I2C:   ready
DRAM:  1 GiB
MMC:   FSL_SDHC: 0, FSL_SDHC: 1
SF: Detected SST25VF016B with page size 256 Bytes, erase size 4 KiB, total 2 MiB
Display: hdmi:1920x1080M@60 (1920x1080)
In:    serial
Out:   serial
Err:   serial
Net:   Micrel ksz9021 at 6
FEC [PRIME], usb_ether
Hit any key to stop autoboot:  0
=> setenv mmc_bootargs 'setenv bootargs console=ttymxc1,115200 root=/dev/mmcblk1p1 rootfstype=ext4 rw consoleblank=0 loglevel=7'
=> setenv mmc_boot 'run mmc_bootargs;mmc dev 1;ext4load mmc 1:1 0x18000000 imx6q-nitrogen6x.dtb;ext4load mmc 1:1 0x12000000 zImage;bootz 0x12000000 - 0x18000000'            
=> setenv bootcmd 'run mmc_boot'
=> boot
switch to partitions #0, OK
mmc1 is current device
52800 bytes read in 149 ms (345.7 KiB/s)
5463352 bytes read in 406 ms (12.8 MiB/s)
Kernel image @ 0x12000000 [ 0x000000 - 0x535d38 ]
## Flattened Device Tree blob at 18000000
   Booting using the fdt blob at 0x18000000
   Using Device Tree in place at 18000000, end 1800fe3f

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Linux version 4.9.74 (suraj@suraj-ubuntu-lap) (gcc version 7.4.0 (Buildroot 2019.02.5) ) #17 SMP PREEMPT Wed Sep 11 18:20:23 IST 2019
[    0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c5387d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] OF: fdt:Machine model: Boundary Devices i.MX6 Quad Nitrogen6x Board
[    0.000000] Reserved memory: created CMA memory pool at 0x3c000000, size 320 MiB
[    0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[    0.000000] Memory policy: Data cache writealloc
[    0.000000] percpu: Embedded 14 pages/cpu @ab6f9000 s26124 r8192 d23028 u57344
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 260096
[    0.000000] Kernel command line: console=ttymxc1,115200 root=/dev/mmcblk1p1 rootfstype=ext4 rw consoleblank=0 loglevel=7
[    0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[    0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[    0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[    0.000000] Memory: 697680K/1048576K available (8192K kernel code, 366K rwdata, 2100K rodata, 1024K init, 467K bss, 23216K reserved, 327680K cma-reserved, 0K highmem)
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[    0.000000]     fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
[    0.000000]     vmalloc : 0xc0800000 - 0xff800000   (1008 MB)
[    0.000000]     lowmem  : 0x80000000 - 0xc0000000   (1024 MB)
[    0.000000]     pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)
[    0.000000]     modules : 0x7f000000 - 0x7fe00000   (  14 MB)
[    0.000000]       .text : 0x80008000 - 0x80900000   (9184 kB)
[    0.000000]       .init : 0x80c00000 - 0x80d00000   (1024 kB)
[    0.000000]       .data : 0x80d00000 - 0x80d5ba00   ( 367 kB)
[    0.000000]        .bss : 0x80d5d000 - 0x80dd1ec4   ( 468 kB)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[    0.000000] Preemptible hierarchical RCU implementation.
[    0.000000]  Build-time adjustment of leaf fanout to 32.
[    0.000000] NR_IRQS:16 nr_irqs:16 16
[    0.000000] L2C-310 errata 752271 769419 enabled
[    0.000000] L2C-310 enabling early BRESP for Cortex-A9
[    0.000000] L2C-310 full line of zeros enabled for Cortex-A9
[    0.000000] L2C-310 ID prefetch enabled, offset 16 lines
[    0.000000] L2C-310 dynamic clock gating enabled, standby mode enabled
[    0.000000] L2C-310 cache controller enabled, 16 ways, 1024 kB
[    0.000000] L2C-310: CACHE_ID 0x410000c7, AUX_CTRL 0x76470001
[    0.000000] Switching to timer-based delay loop, resolution 333ns
[    0.000007] sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns
[    0.000027] clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns
[    0.001626] Console: colour dummy device 80x30
[    0.001647] Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
[    0.001664] pid_max: default: 32768 minimum: 301
[    0.001736] Security Framework initialized
[    0.001747] Yama: becoming mindful.
[    0.001788] AppArmor: AppArmor initialized
[    0.001828] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[    0.001840] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[    0.002432] CPU: Testing write buffer coherency: ok
[    0.002810] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[    0.002872] Setting up static identity map for 0x10100000 - 0x10100058
[    0.169787] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[    0.239777] CPU2: thread -1, cpu 2, socket 0, mpidr 80000002
[    0.309778] CPU3: thread -1, cpu 3, socket 0, mpidr 80000003
[    0.309886] Brought up 4 CPUs
[    0.309913] SMP: Total of 4 processors activated (24.00 BogoMIPS).
[    0.309924] CPU: All CPU(s) started in SVC mode.
[    0.310759] devtmpfs: initialized
[    0.325185] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
[    0.325507] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[    0.325532] futex hash table entries: 1024 (order: 4, 65536 bytes)
[    0.342220] pinctrl core: initialized pinctrl subsystem
[    0.343439] NET: Registered protocol family 16
[    0.353029] DMA: preallocated 256 KiB pool for atomic coherent allocations
[    0.389533] cpuidle: using governor menu
[    0.389720] CPU identified as i.MX6Q, silicon rev 1.2
[    0.419991] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
[    0.420008] hw-breakpoint: maximum watchpoint size is 4 bytes.
[    0.421320] imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
[    0.424047] imx-gpc 20dc000.gpc: no fsl,ldo-bypass found!
[    0.424195] imx-gpc 20dc000.gpc: Registered imx-gpc
[    0.486632] mxs-dma 110000.dma-apbh: initialized
[    0.490160] 2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 28, base_baud = 5000000) is a IMX
[    0.491066] 21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 77, base_baud = 5000000) is a IMX
[    0.954415] console [ttymxc1] enabled
[    0.958721] 21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 78, base_baud = 5000000) is a IMX
[    0.968602] SCSI subsystem initialized
[    0.972885] usbcore: registered new interface driver usbfs
[    0.978448] usbcore: registered new interface driver hub
[    0.983887] usbcore: registered new device driver usb
[    0.989161] 2000000.aips-bus:usbphy_nop1 supply vcc not found, using dummy regulator
[    0.997080] 2000000.aips-bus:usbphy_nop2 supply vcc not found, using dummy regulator
[    1.005631] imx-i2c 21a0000.i2c: stop-delay=0, inter-byte-delay=0
[    1.012276] i2c i2c-0: IMX I2C adapter registered
[    1.017004] i2c i2c-0: can't use DMA, using PIO instead.
[    1.022769] imx-i2c 21a4000.i2c: stop-delay=0, inter-byte-delay=0
[    1.029612] i2c i2c-1: IMX I2C adapter registered
[    1.034337] i2c i2c-1: can't use DMA, using PIO instead.
[    1.040036] imx-i2c 21a8000.i2c: stop-delay=0, inter-byte-delay=0
[    1.047331] i2c i2c-2: IMX I2C adapter registered
[    1.052086] i2c i2c-2: can't use DMA, using PIO instead.
[    1.057889] Linux video capture interface: v2.00
[    1.062583] pps_core: LinuxPPS API ver. 1 registered
[    1.067557] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>
[    1.076735] PTP clock support registered
[    1.109536] imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
[    1.139534] imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
[    1.148613] mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 driver probed
[    1.155357] mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 dphy version is 0x3130302a
[    1.163318] MIPI CSI2 driver module loaded
[    1.167875] imx rpmsg driver is registered.
[    1.172276] Advanced Linux Sound Architecture Driver Initialized.
[    1.179701] Bluetooth: Core ver 2.22
[    1.183322] NET: Registered protocol family 31
[    1.187775] Bluetooth: HCI device and connection manager initialized
[    1.194170] Bluetooth: HCI socket layer initialized
[    1.199066] Bluetooth: L2CAP socket layer initialized
[    1.204180] Bluetooth: SCO socket layer initialized
[    1.209081] NetLabel: Initializing
[    1.212514] NetLabel:  domain hash size = 128
[    1.216878] NetLabel:  protocols = UNLABELED CIPSOv4
[    1.221922] NetLabel:  unlabeled traffic allowed by default
[    1.228030] clocksource: Switched to clocksource mxc_timer1
[    1.233755] VFS: Disk quotas dquot_6.6.0
[    1.237754] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[    1.245067] AppArmor: AppArmor Filesystem Enabled
[    1.262653] NET: Registered protocol family 2
[    1.267673] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[    1.274836] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[    1.281425] TCP: Hash tables configured (established 8192 bind 8192)
[    1.287857] UDP hash table entries: 512 (order: 2, 16384 bytes)
[    1.293846] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[    1.300421] NET: Registered protocol family 1
[    1.305291] RPC: Registered named UNIX socket transport module.
[    1.311247] RPC: Registered udp transport module.
[    1.315958] RPC: Registered tcp transport module.
[    1.320689] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    1.327640] hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
[    1.337921] Bus freq driver module loaded
[    1.343159] audit: initializing netlink subsys (disabled)
[    1.348640] audit: type=2000 audit(1.280:1): initialized
[    1.354927] workingset: timestamp_bits=30 max_order=18 bucket_order=0
[    1.368734] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[    1.376058] NFS: Registering the id_resolver key type
[    1.381172] Key type id_resolver registered
[    1.385367] Key type id_legacy registered
[    1.389658] fuse init (API version 7.26)
[    1.400481] io scheduler noop registered
[    1.404421] io scheduler deadline registered
[    1.408917] io scheduler cfq registered (default)
[    1.416192] OF: PCI: host bridge /soc/pcie@0x01000000 ranges:
[    1.422026] OF: PCI:   No bus range found for /soc/pcie@0x01000000, using [bus 00-ff]
[    1.429912] OF: PCI:    IO 0x01f80000..0x01f8ffff -> 0x00000000
[    1.435855] OF: PCI:   MEM 0x01000000..0x01efffff -> 0x01000000
[    1.650745] imx6q-pcie 1ffc000.pcie: phy link never came up
[    1.656333] imx6q-pcie 1ffc000.pcie: Link never came up
[    1.664669] imx6q-pcie 1ffc000.pcie: failed to initialize host
[    1.670600] imx6q-pcie: probe of 1ffc000.pcie failed with error -110
[    1.685330] 20e0000.hdmi_video supply HDMI not found, using dummy regulator
[    1.694739] add tfp410 i2c driver
[    1.702018] imx-sdma 20ec000.sdma: no iram assigned, using external mem
[    1.709099] imx-sdma 20ec000.sdma: loaded firmware 3.3
[    1.721031] imx sema4 driver is registered.
[    1.725287] [drm] Initialized
[    1.728804] [drm] Initialized vivante 1.0.0 20120216 on minor 0
[    1.747364] brd: module loaded
[    1.757966] loop: module loaded
[    1.761321] [max77823_init] start
[    1.766114] ahci-imx 2200000.sata: fsl,transmit-level-mV not specified, using 00000024
[    1.774082] ahci-imx 2200000.sata: fsl,transmit-boost-mdB not specified, using 00000480
[    1.782155] ahci-imx 2200000.sata: fsl,transmit-atten-16ths not specified, using 00002000
[    1.790385] ahci-imx 2200000.sata: fsl,receive-eq-mdB not specified, using 05000000
[    1.801930] ahci-imx 2200000.sata: SSS flag set, parallel bus scan disabled
[    1.808961] ahci-imx 2200000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
[    1.817766] ahci-imx 2200000.sata: flags: ncq sntf stag pm led clo only pmp pio slum part ccc apst
[    1.828282] scsi host0: ahci-imx
[    1.831882] ata1: SATA max UDMA/133 mmio [mem 0x02200000-0x02203fff] port 0x100 irq 85
[    1.843227] m25p80 spi0.0: sst25vf016b (2048 Kbytes)
[    1.848272] 3 ofpart partitions found on MTD device spi0.0
[    1.853768] Creating 3 MTD partitions on "spi0.0":
[    1.858596] 0x000000000000-0x0000000c0000 : "U-Boot"
[    1.864969] 0x0000000c0000-0x0000000c2000 : "env"
[    1.870970] 0x0000000c2000-0x000000200000 : "splash"
[    1.877260] spi_imx 2008000.ecspi: probed
[    1.882322] libphy: Fixed MDIO Bus: probed
[    1.886877] CAN device driver interface
[    1.891098] 2090000.flexcan supply xceiver not found, using dummy regulator
[    1.899077] flexcan 2090000.flexcan: device registered (reg_base=c0b14000, irq=36)
[    1.908224] 2188000.ethernet supply phy not found, using dummy regulator
[    1.915518] pps pps0: new PPS source ptp0
[    1.920785] libphy: fec_enet_mii_bus: probed
[    1.925073] mdio_bus 2188000.ethernet-1: /soc/aips-bus@02100000/ethernet@02188000/mdio/ethernet-phy has invalid PHY address
[    1.948656] fec 2188000.ethernet eth0: registered PHC device 0
[    1.954860] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[    1.961426] ehci-pci: EHCI PCI platform driver
[    1.966019] usbcore: registered new interface driver cdc_acm
[    1.971746] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
[    1.979866] usbcore: registered new interface driver usb-storage
[    1.985994] usbcore: registered new interface driver usbserial
[    1.991937] usbcore: registered new interface driver usbserial_generic
[    1.998543] usbserial: USB Serial support registered for generic
[    2.004604] usbcore: registered new interface driver cp210x
[    2.010279] usbserial: USB Serial support registered for cp210x
[    2.016249] usbcore: registered new interface driver ftdi_sio
[    2.022067] usbserial: USB Serial support registered for FTDI USB Serial Device
[    2.029471] usbcore: registered new interface driver keyspan
[    2.035178] usbserial: USB Serial support registered for Keyspan - (without firmware)
[    2.043078] usbserial: USB Serial support registered for Keyspan 1 port adapter
[    2.050457] usbserial: USB Serial support registered for Keyspan 2 port adapter
[    2.057822] usbserial: USB Serial support registered for Keyspan 4 port adapter
[    2.065251] usbcore: registered new interface driver pl2303
[    2.070892] usbserial: USB Serial support registered for pl2303
[    2.076860] usbcore: registered new interface driver qcserial
[    2.082672] usbserial: USB Serial support registered for Qualcomm USB modem
[    2.091360] 2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
[    2.099723] setup_reset_gpios:-2, flags 0
[    2.109535] setup_reset_gpios:204, flags 1
[    2.138078] setup_reset_gpios:-2, flags 1
[    2.142240] 2184200.usb supply vbus not found, using dummy regulator
[    2.151964] ci_hdrc ci_hdrc.1: EHCI Host Controller
[    2.156879] ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
[    2.169724] ata1: SATA link down (SStatus 0 SControl 300)
[    2.175170] ahci-imx 2200000.sata: no device found, disabling link.
[    2.181481] ahci-imx 2200000.sata: pass ahci_imx..hotplug=1 to enable hotplug
[    2.188071] ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
[    2.189067] hub 1-0:1.0: USB hub found
[    2.189113] hub 1-0:1.0: 1 port detected
[    2.190356] mousedev: PS/2 mouse device common for all mice
[    2.192204] check_alarm_past: alarm in the past
[    2.192440] snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as rtc0
[    2.192622] i2c /dev entries driver
[    2.195931] imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)
[    2.196685] device-mapper: ioctl: 4.35.0-ioctl (2016-06-23) initialised: [email protected]
[    2.197533] sdhci: Secure Digital Host Controller Interface driver
[    2.197537] sdhci: Copyright(c) Pierre Ossman
[    2.197541] sdhci-pltfm: SDHCI platform and OF driver helper
[    2.358053] mmc2: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
[    2.365790] sdhci-esdhc-imx 2198000.usdhc: could not get ultra high speed state, work on normal mode
[    2.398088] sdhci-esdhc-imx 2198000.usdhc: Got CD GPIO
[    2.478195] mmc0: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
[    2.485963] sdhci-esdhc-imx 219c000.usdhc: could not get ultra high speed state, work on normal mode
[    2.498104] sdhci-esdhc-imx 219c000.usdhc: Got CD GPIO
[    2.568307] mmc1: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA
[    2.577521] mxc_vpu 2040000.vpu_fsl: VPU initialized
[    2.588505] mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
[    2.597842] caam 2100000.caam: ERA source: CAAMVID.
[    2.602831] caam 2100000.caam: AXI pipeline throttling enabled.
[    2.610059] caam 2100000.caam: Entropy delay = 3200
[    2.656132] mmc1: host does not support reading read-only switch, assuming write-enable
[    2.670443] mmc1: new high speed SDXC card at address 59b4
[    2.675775] caam 2100000.caam: Instantiated RNG4 SH0
[    2.681545] mmcblk1: mmc1:59b4 00000 59.7 GiB
[    2.687639]  mmcblk1: p1
[    2.736536] caam 2100000.caam: Instantiated RNG4 SH1
[    2.741544] caam 2100000.caam: device ID = 0x0a16010000000000 (Era 4)
[    2.747999] caam 2100000.caam: job rings = 2, qi = 0
[    2.760386] caam algorithms registered in /proc/crypto
[    2.770011] caam_jr 2101000.jr0: registering rng-caam
[    2.776122] usbcore: registered new interface driver usbhid
[    2.781738] usbhid: USB HID core driver
[    2.788053] sgtl5000 0-000a: sgtl5000 revision 0x11
[    2.794702] sgtl5000 0-000a: Using internal LDO instead of VDDD: check ER1
[    2.829927] random: fast init done
[    2.834217] fsl-ssi-dai 2028000.ssi: No cache defaults, reading back from HW
[    2.841767] fsl-ssi-dai 202c000.ssi: No cache defaults, reading back from HW
[    2.864503] imx-sgtl5000 sound: sgtl5000 <-> 2028000.ssi mapping ok
[    2.872215] imx-sgtl5000 sound: ASoC: Cannot get gpio at index 0: -2
[    2.878962] NET: Registered protocol family 26
[    2.884021] NET: Registered protocol family 10
[    2.889654] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[    2.896348] NET: Registered protocol family 17
[    2.900844] can: controller area network core (rev 20120528 abi 9)
[    2.907242] NET: Registered protocol family 29
[    2.911733] can: raw protocol (rev 20120528)
[    2.916017] can: broadcast manager protocol (rev 20161123 t)
[    2.921712] can: netlink gateway (rev 20130117) max_hops=1
[    2.927473] Bluetooth: RFCOMM TTY layer initialized
[    2.932398] Bluetooth: RFCOMM socket layer initialized
[    2.937565] Bluetooth: RFCOMM ver 1.11
[    2.941357] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[    2.946682] Bluetooth: BNEP filters: protocol multicast
[    2.951942] Bluetooth: BNEP socket layer initialized
[    2.956980] 8021q: 802.1Q VLAN Support v1.8
[    2.961877] rfkill_gpio bt_rfkill: bt_rfkill device registered.
[    2.967948] Key type dns_resolver registered
[    2.974656] cpu cpu0: Registered imx6q-cpufreq
[    2.979268] Registering SWP/SWPB emulation handler
[    2.984782] AppArmor: AppArmor sha1 policy hashing enabled
[    3.004887] imx_thermal 2000000.aips-bus:tempmon: Automotive CPU temperature grade - max:125C critical:120C passive:115C
[    3.016115] snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:04:54 UTC (294)
[    3.026226] usb_otg_vbus: disabling
[    3.029754] ALSA device list:
[    3.032734]   #0: sgtl5000-audio
[    3.382736] EXT4-fs (mmcblk1p1): recovery complete
[    3.393561] EXT4-fs (mmcblk1p1): mounted filesystem with ordered data mode. Opts: (null)
[    3.401724] VFS: Mounted root (ext4 filesystem) on device 179:33.
[    3.407976] devtmpfs: mounted
[    3.413813] Freeing unused kernel memory: 1024K
[    3.531297] EXT4-fs (mmcblk1p1): re-mounted. Opts: data=ordered
[    3.538099] usb 1-1: new high-speed USB device number 2 using ci_hdrc
Starting syslogd: OK
Starting klogd: OK
Initializing random number generator... done.
Starting network: OK

[    3.765764] hub 1-1:1.0: USB hub found
[    3.769701] hub 1-1:1.0: 3 ports detected
Welcome to Buildroot
buildroot login: root

Thanks in advance.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,412件の閲覧回数
gary_bisson
Senior Contributor III

Hi,

Are you still facing this issue?

Regards,

Gary

0 件の賞賛
返信

2,412件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Surajkumar Mokhasi,

The i.MX6Q SABRELite is manufactured and supported by Boundary Devices. You don’t mention which BSP you are using but I would use the recommended BSP by Boundary Devices and I would contact them if the image is having problems login in.

My apologies for the inconvenience,

Regards.

0 件の賞賛
返信