Connect a GP OUT pin to a GP IN pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Connect a GP OUT pin to a GP IN pin

ソリューションへジャンプ
392件の閲覧回数
vix
Contributor II

I've been using a i.MX8M Plus processor and I have a set of General Purpose Output pins that I drive high or low.

Sometimes, for some specific projects I need to be sure that the voltage level on the pin is at the expected level (to detect short circuits, or faults external to the processor).

One common solution is connecting every GP out pin to another pin configured as GP input.

And read the voltage level of the GP input pins.

This connection can be done externally to the NXP processor, using some resistors.

 

Is there a way to configure the IOMUX so that this kind of connection is done internally to the NXP pricessor?

This would save space on the PCB, and it would be a flexible way to get the same result.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
373件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @vix!
Thank you for contacting NXP Support!

Sorry, that is not possible!

You can use only one GP input with a pull-up internal resistor and read the value.

Sorry for the mistake!

Best Regards!

Chavira

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
374件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @vix!
Thank you for contacting NXP Support!

Sorry, that is not possible!

You can use only one GP input with a pull-up internal resistor and read the value.

Sorry for the mistake!

Best Regards!

Chavira

0 件の賞賛
返信