Configuring chip select as GPIO to control it manually in imx7d

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Configuring chip select as GPIO to control it manually in imx7d

22,076 次查看
koilarulraj
Contributor III

Hi all,

We are working on a device connected to ecspi3 interface of imx7d sabre sd board. We tried to read the chip version from the module but the transaction always returns zero. After debugging the we found that chip select(NSS) should be held down for 16 clock cycles in order to read data from the module but in imx7 the chip select line becomes high after transferring 8 bits. Attached the image of SPI transaction expected by our device,Untitled.png

To avoid this we configured chip select as gpio and tried to control it manually from our driver code. But with this method we are not receiving any clock from the master. Here is our device tree entry.

&ecspi3 {

fsl,spi-num-chipselects = <1>;

pinctrl-names = "default";

pinctrl-0 = <&pinctrl_ecspi3 &pinctrl_ecspi3_cs>;

pinctrl-0 = <&pinctrl_ecspi3>;

/*cs-gpios = <&gpio6 22 GPIO_ACTIVE_HIGH>;*/            NOTE: Commented the cs-gpios entry

/*cs-gpios = <0>;*/                                                                NOTE: Tried this entry also without this entry

status = "okay";

                 spidev0: spi@0 {

                 compatible = "rfm95";

                 reg = <0>;

                 spi-max-frequency = <4000000>;

                 interrupt-parent = <&gpio2>;

                 interrupts = <11 1>;

                 cs-gpio = <&gpio6 22 GPIO_ACTIVE_HIGH>;  NOTE: Used this gpio for Chip select from our driver.

                 intr-gpio = <&gpio2 11 GPIO_ACTIVE_HIGH>;

                 rst-gpio = <&gpio2 10 GPIO_ACTIVE_HIGH>;

                 enable-gpio = <&gpio2 0 GPIO_ACTIVE_HIGH>;

             };

}

RESULT:

On doing this the chip select line toggles, but there is not clock from the SCLK line.

So,

1. Is there anything we missed to configure chip select as gpio?

2.Is there any patch available for 4.9.11 kernel to configure chip select as gpio to control it in iMX7D?

3. Is there any working patch available to avoid SPI controller(spi-imx.c) toggling chip select after transferring 8 bits?

Thanks,

Koil Arul Raj S

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

20,928 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Koil

using "cs-gpios" in dts, kernel configures ecspi chip select as gpio,

for holding chip select for 16 clock cycles one can try to configure

field BURST_LENGTH register ECSPIx_CONREG, described in

sect.10.1.7.3 Control Register (ECSPIx_CONREG) i.MX7D Reference Manual

http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf

Linux spi driver is described in sect.4.4 Enhanced Configurable Serial Peripheral Interface
(ECSPI) attached Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复