Configuring EIM for ADV7391

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Configuring EIM for ADV7391

ソリューションへジャンプ
2,684件の閲覧回数
aliismail
Contributor IV

I am currently working on integrating the ADV7391 with the i.MX6 SCM. I have followed along

https://community.nxp.com/docs/DOC-94019

and applied all the patches for the 3.14.52 kernel. I am currently running into the issue where I do not see a 27 MHz clock coming from the EIM to the ADV7391. I have configured my device device tree as follows.

imx6qdl-sabresd {
   pinctrl_ipu1_bt656: ipu1grp-3 {
      fsl,pins = <
         MX6QDL_PAD_EIM_A16__IPU1_DI1_DISP_CLK 0x10
         MX6QDL_PAD_EIM_DA9__IPU1_DISP1_DATA00 0x10
         MX6QDL_PAD_EIM_DA8__IPU1_DISP1_DATA01 0x10
         MX6QDL_PAD_EIM_DA7__IPU1_DISP1_DATA02 0x10
         MX6QDL_PAD_EIM_DA6__IPU1_DISP1_DATA03 0x10
         MX6QDL_PAD_EIM_DA5__IPU1_DISP1_DATA04 0x10
         MX6QDL_PAD_EIM_DA4__IPU1_DISP1_DATA05 0x10
         MX6QDL_PAD_EIM_DA3__IPU1_DISP1_DATA06 0x10
         MX6QDL_PAD_EIM_DA2__IPU1_DISP1_DATA07 0x10
         >;
      };
};

I have also created a patch to modify the IPU1_DI1_DISP_CLK to 27 MHz.

--- a/arch/arm/mach-imx/clk-imx6q.c
+++ b/arch/arm/mach-imx/clk-imx6q.c
@@ -792,7 +792,7 @@ static void __init imx6q_clocks_init(struct device_node *ccm_node)
}
/* ipu clock initialization */
imx_clk_set_parent(clk[IMX6QDL_CLK_IPU1_DI0_PRE_SEL], clk[IMX6QDL_CLK_PLL5_VIDEO_DIV]);
- imx_clk_set_parent(clk[IMX6QDL_CLK_IPU1_DI1_PRE_SEL], clk[IMX6QDL_CLK_PLL5_VIDEO_DIV]);
+ imx_clk_set_parent(clk[IMX6QDL_CLK_IPU1_DI1_PRE_SEL], clk[IMX6QDL_CLK_PLL3_PFD1_540M]); /* For CVBS 27MHz clock */
imx_clk_set_parent(clk[IMX6QDL_CLK_IPU2_DI0_PRE_SEL], clk[IMX6QDL_CLK_PLL5_VIDEO_DIV]);
imx_clk_set_parent(clk[IMX6QDL_CLK_IPU2_DI1_PRE_SEL], clk[IMX6QDL_CLK_PLL5_VIDEO_DIV]);
imx_clk_set_parent(clk[IMX6QDL_CLK_IPU1_DI0_SEL], clk[IMX6QDL_CLK_IPU1_DI0_PRE]);

I am not sure what else I am missing to ensure that the EIM provides the correct clock?

ラベル(4)
0 件の賞賛
返信
1 解決策
2,342件の閲覧回数
aliismail
Contributor IV

Thanks for the reply Alejandro. It looks like my device tree settings were not getting configured properly.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,343件の閲覧回数
aliismail
Contributor IV

Thanks for the reply Alejandro. It looks like my device tree settings were not getting configured properly.

0 件の賞賛
返信
2,342件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Have you checked that the "clocks" property in the device tree is the correct. 

The parent configuration seems to be ok, but to double check you can use the below command to check the clock tree:

> cat /sys/kernel/debug/clk/clk_summary:l/debug/clk/clk_summary

There might be at some point of the code where  a clk_prepare_enable is called to enable the corresponding clock. 

This might happen in the ADV7391 driver of the clk-imx6q.c. 

Also you can use the memtool to check the IOMUXC and see if the PAD is configured with the correct alternative. 

> unit_tests/memtool IOMUXC.SW_MUX_CTL_PAD_EIM_A16

Best Regards,

Alejandro