Configure external PMIC for Normal ON to OFF by button

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Configure external PMIC for Normal ON to OFF by button

4,841 Views
AMBh
Contributor I

Hi team,

I am using Imx8-Mini controller in my application and want to configure the external PMIC for Normal Power mode transition ON to Off by button. But I could not able to find the descriptive way to do that.

Can you propose the solution for it?

 

 

0 Kudos
Reply
6 Replies

4,790 Views
AMBh
Contributor I

Hi @Chavira 

We have used the same schematic and connections. And also used provided dts file by NXP.

But still i could not able to get interrupt on IRQ line.

As per the attached image I want to use Normal ON/OFF by button Power Mode when the configuration of PMIC is externel so that I could able to get interrupt on IRQ.

Can you provide me steps how to get POWER On/Off short press and long press interrupt. Currently after long press board is turned off.

0 Kudos
Reply

4,769 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @AMBh !

You can base your schematic using our design.

 

I recommend checking the PMIC signals with an oscilloscope to see what is wrong, I think the root cause could be your design and not the software.

 

We don´t have step by step manual but the schematic is enough to understand the signals and how are connected.

 

Sorry for the mistake!

 

Best Regards!

Chavira

0 Kudos
Reply

4,743 Views
AMBh
Contributor I

Hi,

Schematics are base on NXP eval board only.

I could not able to understand how to enable interrupt so that I would get interrupt on PMIC_nINT line.

Is any guidelines for that?

0 Kudos
Reply

4,728 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @AMBh!

Sorry, we don't have any documents.

The PMIC_ON_REQ is generated by the IMX8MM and if you follow the schematic should work fine.

Please check the chapter "6.5.2.1 Reset and Power-up Flow" that explains how to work the power on/off button and how that button activates the PMIC_ON_REQ to start the power on/off sequence.

Best Regards!
Chavira

0 Kudos
Reply

4,692 Views
AMBh
Contributor I

Yes you were right, I can turn OFF and ON the board.

But now if as per the below screenshot 

AMBh_0-1695894707732.png

Can we check the irq status in user space which was sent to SOC by FSM after button press?

If yes then how?

 

0 Kudos
Reply

4,819 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @AMBh!


Thank you for contacting NXP Support!

We have a board with a power/off button you can download the schematic files to see the connections made for that purpose

Please download the design files by following the link:

https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/evaluation-kit-...


Best Regards!

Chavira

0 Kudos
Reply