Config PWM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Config PWM

1,299 Views
IanBrand
Contributor I

Hi NXP,

How to configure 7 and 4 pins to output PWM signals respectively? [i.MX RT 1020 ]

0 Kudos
Reply
1 Reply

1,234 Views
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

That pins corresponds to PWM_X signals, which can output a third PWM signal from each submodule. However, the SDK does not include support for PWM_X functionality other than input capture.

If you refer to the 50.3.2.4 PWM Generation section of reference manual, the VAL0 and VAL1 comparators can be used to set frequency and duty cycle, based on the incoming clock to the counter.

Hope it helps you.

Have a nice day!

0 Kudos
Reply