Compiling kobs-ng_v5.5 Failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Compiling kobs-ng_v5.5 Failed

1,317 Views
jasonshao
Contributor II

I have got the source code of imx-kobs version 5.5 from GitHub - codeauroraforum/imx-kobs: Tool to create and write Freescale/NXP I.MX NAND boot related boo... ,and configured as this:

./configure CC=arm-none-linux-gnueabi-gcc --host=arm-none-linux-gnueabi-gcc. But when I compiled it, I got ERR like this

pastedImage_3.png

Who can help?

Labels (2)
0 Kudos
Reply
1 Reply

1,247 Views
b36401
NXP Employee
NXP Employee

It seems the is some mis-versioning in the sources you are compiling.
Please try to re-get the sources with an accuracy.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply