Compiling a Linux Kernel with GPU and VPU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Compiling a Linux Kernel with GPU and VPU

2,362 Views
jorgebarrios
Contributor I

Hi, I´m a student from PADTS CINVESTAV GUADALAJARA, MEX:. I would like to know if someone could help me with a step by step tutorial about compiling a Linux Kernel (as minimal as it could be) with GPU and VPU support (i need to include X11 or directFB libraries as well).

Also I would like to know if i could build it without using LTIB tool because I have tried it a lot of times and i got the same error.

I´m a not very experienced user of Linux.

Hola, soy estudiante de EMBEDDED SOFTWARE -PADTS-13 en CINVESTAV unidad Guadalajara, Mex. ¿Me podrían ayudar con un tutorial de cómo compilar un Kernel de Linux (lo mas mínimo posible) con soporte para GPU y VPU (con soporte de librerías X11 o directFB)? también me gustaría saber si se puede hacer sin necesidad de utilizar LTIB puesto que ya lo he intentado y me aparece un error, lo intente en varias ocasiones y lo mismo.

Labels (1)
0 Kudos
Reply
3 Replies

2,209 Views
LeonardoSandova
Specialist I

what error are you having? Please post the error log

Leo

0 Kudos
Reply

2,209 Views
jorgebarrios
Contributor I

ErrorLTIB.PNG

0 Kudos
Reply

2,209 Views
LeonardoSandova
Specialist I

I know that an image is more than a thousands words :smileyhappy: but please post the whole error log, just copy and paste into a file and attach it.

Leo

0 Kudos
Reply