Compiling Kernel Module in ICS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Compiling Kernel Module in ICS

ソリューションへジャンプ
2,811件の閲覧回数
venkatramangurr
Contributor I

Hi All,

I am currently trying to compile kernel module for a local echo driver in ICS. I got success while trying the same in GB but doing so in ICS the echo driver is not get compiled to KO object

I got below errors while compiling

make circular .so - .so dependency dropped in android

#build/core/main.mk:537: *** Some files have been added to ALL_PREBUILT.

#build/core/main.mk:538: *

#build/core/main.mk:539: * ALL_PREBUILT is a deprecated mechanism that

#build/core/main.mk:540: * should not be used for new files.

#build/core/main.mk:541: * As an alternative, use PRODUCT_COPY_FILES in

#build/core/main.mk:542: * the appropriate product definition.

#build/core/main.mk:543: * build/target/product/core.mk is the product

#build/core/main.mk:544: * definition used in all products.

#build/core/main.mk:545: *

#build/core/main.mk:546: * unexpected circular-char.ko in ALL_PREBUILT

#build/core/main.mk:547: *

#build/core/main.mk:548: *** ALL_PREBUILT contains unexpected files.  Stop.


I know that the problem is in Android.mk of the echo driver source, So please guide me on making make file in ICS


Looking forward for your guidlines....


Regards

Venkatraman


ラベル(2)
タグ(4)
0 件の賞賛
返信
1 解決策
2,334件の閲覧回数
max_tsai
NXP Employee
NXP Employee

I am not sure if you modified ALL_PREBUILT table for your error message.

You can refer to "system/wlan/atheros". It's WiFi module, and built as KO format.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,334件の閲覧回数
max_tsai
NXP Employee
NXP Employee

I am not sure if you modified ALL_PREBUILT table for your error message.

You can refer to "system/wlan/atheros". It's WiFi module, and built as KO format.

0 件の賞賛
返信