Compatibility of i.Mx6Q processor with Redpine wifi module RS9113 for SDIO interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Compatibility of i.Mx6Q processor with Redpine wifi module RS9113 for SDIO interface

1,311 次查看
nanjundam
Contributor II

Hi,

I;m using i.Mx6Q in my design with Wifi module RS9113-N00-D0N.

I want to interface these with SDIO signals.

As per the Datasheets the RS9113 has SDIO 2.0 interface, and i.Mx6Q has SDIO 3.0 interface (SDIO1 will be used).

My question is, are the two parts are compatible with each other ?

Is the SDIO 3.0 of i.Mx6 is backword compatible with SDIO 2.0 of RS9113 wifi module ?

Please reply ASAP.

Thanks & Regards,

Nanjunda M

标签 (3)
标记 (2)
0 项奖励
回复
1 回复

1,051 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Nanjunda

yes i.MX6 SDIO 3.0 is backward compatible with SDIO 2.0, RS9113 wifi module

can be used with i.MX6 processor.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复