Code Aurora unusably slow

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code Aurora unusably slow

3,319 Views
dkley
Contributor II

Navigating around https://source.codeaurora.org/external/imx/linux-imx/ is incredibly slow (or I get 502 errors). Trying to clone the repo (in Yocto and from CLI) seems to hang. I left a clone running over 12+ hours before killing it. I've verified this is the case on multiple connections.

Are there any mirrors available with better performance, or an ETA on a fix for the repository?

 

Traceroute:
...

5: 173-219-197-48.suddenlink.net 25.525ms
6: dls-b23-link.ip.twelve99.net 19.126ms
7: ntt-ic325660-dls-b23.ip.twelve99-cust.net 15.632ms
8: ae-2.r21.dllstx14.us.bb.gin.ntt.net 19.311ms asymm 9
9: ae-2.r25.snjsca04.us.bb.gin.ntt.net 70.373ms asymm 11
10: ae-45.r01.snjsca04.us.bb.gin.ntt.net 81.441ms asymm 9
11: ae-0.taobao.snjsca04.us.bb.gin.ntt.net 87.079ms asymm 9
12: ??? 103.894ms asymm 11

...

5 Replies

3,248 Views
dkley
Contributor II

Checking again today it seems as if the performance issue has been resolved from the US.

0 Kudos
Reply

3,215 Views
dunk
Contributor III

Thanks, dkley.

 

0 Kudos
Reply

3,316 Views
dkley
Contributor II

Seems like this may be related to being located in the US:

https://community.nxp.com/t5/i-MX-Processors/about-kernel-linux-imx-branch/m-p/1068951#M157057

 

Edit -

Going through a VPN in France fixed the problem for me - so definitely a CDN/routing issue in the US.

3,287 Views
dunk
Contributor III

Hi dkley,

Would you share the information of VPN in Franced used in your fixup?

0 Kudos
Reply

3,250 Views
dkley
Contributor II

Hi dunk,

I just used NordVPN with the location specified as France.

0 Kudos
Reply