Chromium & iMX 6Quad & GPU

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Chromium & iMX 6Quad & GPU

跳至解决方案
6,942 次查看
mirkoardinghi1
Contributor IV


I have built chromiun for X11 (yocto fido).

X11 is running with hardware acceleration.

but when I start chromium i have:

/usr/bin/chrome/chrome --user-data-dir=/mnt/ramdisk

[900:900:0411/122848:ERROR:gl_surface_glx.cc(637)] glXChooseFBConfig failed.

[900:900:0411/122848:ERROR:gpu_info_collector.cc(27)] gfx::GLContext::CreateOffscreenGLSurface failed

[900:900:0411/122848:ERROR:gpu_info_collector.cc(89)] Could not create surface for info collection.

[900:900:0411/122848:ERROR:gpu_main.cc(421)] gpu::CollectGraphicsInfo failed (fatal).

[900:900:0411/122848:ERROR:gpu_child_thread.cc(145)] Exiting GPU process due to errors during initialization

Any help??

My configuration:

xorg.conf

Section "Device"

    Identifier  "i.MX Accelerated Framebuffer Device"

    Driver      "vivante"

    Option      "fbdev"     "/dev/fb0"

    Option      "vivante_fbdev" "/dev/fb0"

    Option      "HWcursor"  "false"

EndSection

Section "ServerFlags"

    Option "BlankTime"  "0"

    Option "StandbyTime"  "0"

    Option "SuspendTime"  "0"

    Option "OffTime"  "0"

EndSection

/var/log/Xorg.0.log

[ 83014.362]

X.Org X Server 1.16.3

Release Date: 2014-12-20

[ 83014.362] X Protocol Version 11, Revision 0

[ 83014.362] Build Operating System: Linux 3.13.0-77-generic x86_64

[ 83014.362] Current Operating System: Linux icorem6quad 3.14.28-1.0.0_ga+g91cf351 #1 SMP PREEMPT Mon Apr 11 09:32:49 CEST 2016 armv7l

[ 83014.362] Kernel command line: console=ttymxc3,115200 cma=256MB gpumem=16MB engi_board=SK.RES video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24, mtdparts=gpmi-nand:4m(boot),8m(kernel),1m(dtb),-(rootfs) root=/dev/w

[ 83014.362] Build Date: 08 April 2016  01:57:35PM

[ 83014.362] 

[ 83014.362] Current version of pixman: 0.32.6

[ 83014.362]    Before reporting problems, check http://wiki.x.org

        to make sure that you have the latest version.

[ 83014.362] Markers: (--) probed, (**) from config file, (==) default setting,

        (++) from command line, (!!) notice, (II) informational,

        (WW) warning, (EE) error, (NI) not implemented, (??) unknown.

[ 83014.363] (==) Log file: "/var/log/Xorg.0.log", Time: Mon Apr 11 10:51:35 2016

[ 83014.372] (==) Using config file: "/etc/X11/xorg.conf"

[ 83014.372] (==) Using system config directory "/usr/share/X11/xorg.conf.d"

[ 83014.376] (==) No Layout section.  Using the first Screen section.

[ 83014.376] (==) No screen section available. Using defaults.

[ 83014.376] (**) |-->Screen "Default Screen Section" (0)

[ 83014.376] (**) |   |-->Monitor "<default monitor>"

[ 83014.383] (==) No device specified for screen "Default Screen Section".

        Using the first device section listed.

[ 83014.383] (**) |   |-->Device "i.MX Accelerated Framebuffer Device"

[ 83014.383] (==) No monitor specified for screen "Default Screen Section".

        Using a default monitor configuration.

[ 83014.383] (**) Option "BlankTime" "0"

[ 83014.383] (**) Option "StandbyTime" "0"

[ 83014.383] (**) Option "SuspendTime" "0"

[ 83014.383] (**) Option "OffTime" "0"

[ 83014.383] (==) Automatically adding devices

[ 83014.383] (==) Automatically enabling devices

[ 83014.383] (==) Automatically adding GPU devices

[ 83014.384] (WW) The directory "/usr/share/fonts/X11/misc/" does not exist.

[ 83014.384]    Entry deleted from font path.

[ 83014.384] (WW) The directory "/usr/share/fonts/X11/TTF/" does not exist.

[ 83014.384]    Entry deleted from font path.

[ 83014.384] (WW) The directory "/usr/share/fonts/X11/OTF/" does not exist.

[ 83014.384]    Entry deleted from font path.

[ 83014.384] (WW) The directory "/usr/share/fonts/X11/Type1/" does not exist.

[ 83014.384]    Entry deleted from font path.

[ 83014.384] (WW) The directory "/usr/share/fonts/X11/100dpi/" does not exist.

[ 83014.384]    Entry deleted from font path.

[ 83014.384] (WW) The directory "/usr/share/fonts/X11/75dpi/" does not exist.

[ 83014.384]    Entry deleted from font path.

[ 83014.384] (==) FontPath set to:

[ 83014.384] (==) ModulePath set to "/usr/lib/xorg/modules"

[ 83014.384] (II) The server relies on udev to provide the list of input devices.

        If no devices become available, reconfigure udev or disable AutoAddDevices.

[ 83014.385] (II) Loader magic: 0x1b2bd8

[ 83014.385] (II) Module ABI versions:

[ 83014.385]    X.Org ANSI C Emulation: 0.4

[ 83014.385]    X.Org Video Driver: 18.0

[ 83014.385]    X.Org XInput driver : 21.0

[ 83014.385]    X.Org Server Extension : 8.0

[ 83014.386] (II) xfree86: Adding drm device (/dev/dri/card0)

[ 83014.387] (II) no primary bus or device found

[ 83014.387]    falling back to /sys/devices/platform/Vivante GCCore/drm/card0

[ 83014.388] (II) LoadModule: "glx"

[ 83014.392] (II) Loading /usr/lib/xorg/modules/extensions/libglx.so

[ 83014.508] (II) Module glx: vendor="X.Org Foundation"

[ 83014.508]    compiled for 1.16.3, module version = 1.0.0

[ 83014.508]    ABI class: X.Org Server Extension, version 8.0

[ 83014.508] (==) AIGLX enabled

[ 83014.508] (II) LoadModule: "vivante"

[ 83014.508] (II) Loading /usr/lib/xorg/modules/drivers/vivante_drv.so

[ 83014.517] (II) Module vivante: vendor="X.Org Foundation"

[ 83014.518]    compiled for 1.16.3, module version = 1.0.0

[ 83014.518]    Module class: X.Org Video Driver

[ 83014.518]    ABI class: X.Org Video Driver, version 18.0

[ 83014.518] (II) VIVANTE: driver for vivante fb: VivanteGC500, VivanteGC2100,

        VivanteGCCORE

[ 83014.518] (--) using VT number 1

[ 83014.590] (WW) Falling back to old probe method for vivante

[ 83014.590] (II) Loading sub module "fbdevhw"

[ 83014.590] (II) LoadModule: "fbdevhw"

[ 83014.590] (II) Loading /usr/lib/xorg/modules/libfbdevhw.so

[ 83014.593] (II) Module fbdevhw: vendor="X.Org Foundation"

[ 83014.593]    compiled for 1.16.3, module version = 0.0.2

[ 83014.593]    ABI class: X.Org Video Driver, version 18.0

[ 83014.593] (II) VIVANTE(0): using default device

[ 83014.593] (WW) VGA arbiter: cannot open kernel arbiter, no multi-card support

[ 83014.593] (II) VIVANTE(0): Device preferred mode 'fb0':U:1920x1080p-60

[ 83014.594] (II) VIVANTE(0): Creating default Display subsection in Screen section

        "Default Screen Section" for depth/fbbpp 16/16

[ 83014.594] (==) VIVANTE(0): Depth 16, (==) framebuffer bpp 16

[ 83014.594] (==) VIVANTE(0): RGB weight 565

[ 83014.594] (==) VIVANTE(0): Default visual is TrueColor

[ 83014.594] (==) VIVANTE(0): Using gamma correction (1.0, 1.0, 1.0)

[ 83014.594] (**) VIVANTE(0): Option "fbdev" "/dev/fb0"

[ 83014.594] (II) VIVANTE(0): checking modes against framebuffer device...

[ 83014.594] (II) VIVANTE(0): checking modes against monitor...

[ 83014.594] (II) VIVANTE(0): Use built in mode (bpp 16)

[ 83014.594] (--) VIVANTE(0): Virtual size is 0x0 (pitch 0)

[ 83014.594] (==) VIVANTE(0): DPI set to (96, 96)

[ 83014.594] (II) Loading sub module "fb"

[ 83014.594] (II) LoadModule: "fb"

[ 83014.595] (II) Loading /usr/lib/xorg/modules/libfb.so

[ 83014.605] (II) Module fb: vendor="X.Org Foundation"

[ 83014.605]    compiled for 1.16.3, module version = 1.0.0

[ 83014.605]    ABI class: X.Org ANSI C Emulation, version 0.4

[ 83014.605] (II) Loading sub module "exa"

[ 83014.605] (II) LoadModule: "exa"

[ 83014.605] (II) Loading /usr/lib/xorg/modules/libexa.so

[ 83014.621] (II) Module exa: vendor="X.Org Foundation"

[ 83014.621]    compiled for 1.16.3, module version = 2.6.0

[ 83014.621]    ABI class: X.Org Video Driver, version 18.0

[ 83014.738] (II) VIVANTE(0): printing discovered frame buffer 'fb0' supported modes:

[ 83014.739] (II) VIVANTE(0): Modeline "U:640x480p-59"x0.0   25.18  640 656 752 800  480 490 492 525 -hsync -vsync -csync (31.5 kHz e)

[ 83014.739] (II) VIVANTE(0): Modeline "U:1280x720p-120"x0.0  148.50  1280 1390 1430 1650  720 725 730 750 +hsync +vsync -csync (90.0 kHz e)

[ 83014.739] (II) VIVANTE(0): Modeline "U:1280x720p-100"x0.0  148.50  1280 1720 1760 1980  720 725 730 750 +hsync +vsync -csync (75.0 kHz e)

[ 83014.740] (II) VIVANTE(0): Modeline "U:1920x1080p-30"x0.0   74.25  1920 2008 2052 2200  1080 1084 1089 1125 +hsync +vsync -csync (33.8 kHz e)

[ 83014.740] (II) VIVANTE(0): Modeline "U:1920x1080p-25"x0.0   74.25  1920 2448 2492 2640  1080 1084 1089 1125 +hsync +vsync -csync (28.1 kHz e)

[ 83014.740] (II) VIVANTE(0): Modeline "U:1920x1080p-24"x0.0   74.25  1920 2558 2602 2750  1080 1084 1089 1125 +hsync +vsync -csync (27.0 kHz e)

[ 83014.741] (II) VIVANTE(0): Modeline "U:1920x1080p-50"x0.0  148.50  1920 2448 2492 2640  1080 1084 1089 1125 +hsync +vsync -csync (56.2 kHz e)

[ 83014.741] (II) VIVANTE(0): Modeline "U:1440x576p-50"x0.0   54.00  1440 1464 1592 1728  576 581 586 625 -hsync -vsync -csync (31.3 kHz e)

[ 83014.742] (II) VIVANTE(0): Modeline "U:1440x576p-50"x0.0   54.00  1440 1464 1592 1728  576 581 586 625 -hsync -vsync -csync (31.3 kHz e)

[ 83014.742] (II) VIVANTE(0): Modeline "U:1440x288p-50"x0.0   27.00  1440 1464 1590 1728  288 290 293 312 -hsync -vsync -csync (15.6 kHz e)

[ 83014.743] (II) VIVANTE(0): Modeline "U:1440x288p-50"x0.0   27.00  1440 1464 1590 1728  288 290 293 312 -hsync -vsync -csync (15.6 kHz e)

[ 83014.743] (II) VIVANTE(0): Modeline "U:1280x720p-50"x0.0   74.25  1280 1720 1760 1980  720 725 730 750 +hsync +vsync -csync (37.5 kHz e)

[ 83014.743] (II) VIVANTE(0): Modeline "U:720x576p-50"x0.0   27.00  720 732 796 864  576 581 586 625 -hsync -vsync -csync (31.2 kHz e)

[ 83014.744] (II) VIVANTE(0): Modeline "U:720x576p-50"x0.0   27.00  720 732 796 864  576 581 586 625 -hsync -vsync -csync (31.2 kHz e)

[ 83014.744] (II) VIVANTE(0): Modeline "U:1920x1080p-60"x0.0  148.50  1920 2008 2052 2200  1080 1084 1089 1125 +hsync +vsync -csync (67.5 kHz eP)

[ 83014.744] (II) VIVANTE(0): Modeline "U:1440x480p-60"x0.0   54.05  1440 1472 1596 1716  480 489 495 525 -hsync -vsync -csync (31.5 kHz e)

[ 83014.745] (II) VIVANTE(0): Modeline "U:1440x480p-60"x0.0   54.05  1440 1472 1596 1716  480 489 495 525 -hsync -vsync -csync (31.5 kHz e)

[ 83014.745] (II) VIVANTE(0): Modeline "U:1440x240p-60"x0.0   26.95  1440 1478 1602 1716  240 244 247 262 -hsync -vsync -csync (15.7 kHz e)

[ 83014.745] (II) VIVANTE(0): Modeline "U:1440x240p-60"x0.0   26.95  1440 1478 1602 1716  240 244 247 262 -hsync -vsync -csync (15.7 kHz e)

[ 83014.745] (II) VIVANTE(0): Modeline "U:1280x720p-60"x0.0   74.25  1280 1390 1430 1650  720 725 730 750 +hsync +vsync -csync (45.0 kHz e)

[ 83014.746] (II) VIVANTE(0): Modeline "U:720x480p-60"x0.0   27.00  720 736 798 858  480 489 495 525 -hsync -vsync -csync (31.5 kHz e)

[ 83014.746] (II) VIVANTE(0): Modeline "U:720x480p-60"x0.0   27.00  720 736 798 858  480 489 495 525 -hsync -vsync -csync (31.5 kHz e)

[ 83014.746] (II) VIVANTE(0): Modeline "U:640x480p-60"x0.0   25.17  640 656 752 800  480 490 492 525 -hsync -vsync -csync (31.5 kHz e)

[ 83014.784] (II) VIVANTE(0): Output DISP3 BG - DI1 has no monitor section

[ 83014.784] (II) VIVANTE(0): Printing probed modes for output DISP3 BG - DI1

[ 83014.784] (II) VIVANTE(0): Modeline "U:1920x1080p-60"x60.0  148.50  1920 2008 2052 2200  1080 1084 1089 1125 +hsync +vsync -csync (67.5 kHz eP)

[ 83014.784] (II) VIVANTE(0): Modeline "U:1920x1080p-50"x50.0  148.50  1920 2448 2492 2640  1080 1084 1089 1125 +hsync +vsync -csync (56.2 kHz e)

[ 83014.784] (II) VIVANTE(0): Modeline "U:1920x1080p-30"x30.0   74.25  1920 2008 2052 2200  1080 1084 1089 1125 +hsync +vsync -csync (33.8 kHz e)

[ 83014.784] (II) VIVANTE(0): Modeline "U:1920x1080p-25"x25.0   74.25  1920 2448 2492 2640  1080 1084 1089 1125 +hsync +vsync -csync (28.1 kHz e)

[ 83014.785] (II) VIVANTE(0): Modeline "U:1920x1080p-24"x24.0   74.25  1920 2558 2602 2750  1080 1084 1089 1125 +hsync +vsync -csync (27.0 kHz e)

[ 83014.785] (II) VIVANTE(0): Modeline "U:1280x720p-120"x120.0  148.50  1280 1390 1430 1650  720 725 730 750 +hsync +vsync -csync (90.0 kHz e)

[ 83014.785] (II) VIVANTE(0): Modeline "U:1280x720p-100"x100.0  148.50  1280 1720 1760 1980  720 725 730 750 +hsync +vsync -csync (75.0 kHz e)

[ 83014.785] (II) VIVANTE(0): Modeline "U:1280x720p-50"x50.0   74.25  1280 1720 1760 1980  720 725 730 750 +hsync +vsync -csync (37.5 kHz e)

[ 83014.785] (II) VIVANTE(0): Modeline "U:1280x720p-60"x60.0   74.25  1280 1390 1430 1650  720 725 730 750 +hsync +vsync -csync (45.0 kHz e)

[ 83014.785] (II) VIVANTE(0): Modeline "U:1440x576p-50"x50.0   54.00  1440 1464 1592 1728  576 581 586 625 -hsync -vsync -csync (31.3 kHz e)

[ 83014.785] (II) VIVANTE(0): Modeline "U:1440x480p-60"x60.0   54.05  1440 1472 1596 1716  480 489 495 525 -hsync -vsync -csync (31.5 kHz e)

[ 83014.785] (II) VIVANTE(0): Modeline "U:1440x288p-50"x50.1   27.00  1440 1464 1590 1728  288 290 293 312 -hsync -vsync -csync (15.6 kHz e)

[ 83014.785] (II) VIVANTE(0): Modeline "U:720x576p-50"x50.0   27.00  720 732 796 864  576 581 586 625 -hsync -vsync -csync (31.2 kHz e)

[ 83014.785] (II) VIVANTE(0): Modeline "U:720x480p-60"x59.9   27.00  720 736 798 858  480 489 495 525 -hsync -vsync -csync (31.5 kHz e)

[ 83014.785] (II) VIVANTE(0): Modeline "U:1440x240p-60"x59.9   26.95  1440 1478 1602 1716  240 244 247 262 -hsync -vsync -csync (15.7 kHz e)

[ 83014.785] (II) VIVANTE(0): Modeline "U:640x480p-59"x59.9   25.18  640 656 752 800  480 490 492 525 -hsync -vsync -csync (31.5 kHz e)

[ 83014.785] (II) VIVANTE(0): Modeline "U:640x480p-60"x59.9   25.17  640 656 752 800  480 490 492 525 -hsync -vsync -csync (31.5 kHz e)

[ 83014.785] (II) VIVANTE(0): Output DISP3 BG - DI1 connected

[ 83014.785] (II) VIVANTE(0): Using exact sizes for initial modes

[ 83014.785] (II) VIVANTE(0): Output DISP3 BG - DI1 using initial mode U:1920x1080p-60

[ 83014.785] (II) VIVANTE(0): imxDisplayPreInit: virtual set 1920 x 1080, display width 0

[ 83014.785] (II) VIVANTE(0): FBDevPreInit: adjust display width 1920

[ 83014.785] (**) VIVANTE(0): PreInit done

[ 83014.786] (II) VIVANTE(0): Init mode for fb device

[ 83014.857] (II) VIVANTE(0): hardware: DISP3 BG - DI1 (video memory: 8167kB)

[ 83014.857] (II) VIVANTE(0): FB Start = 0x75e50000  FB Base = 0x75e50000  FB Offset = (nil) FB PhyBase 0x48900000

[ 83014.857] (II) VIVANTE(0): reserve 4177920 bytes for on screen frame buffer; total fb memory size 8363520 bytes; offset of shadow buffer 4177920

[ 83014.915] (II) VIVANTE(0): hardware: DISP3 BG - DI1 (video memory: 8167kB)

[ 83014.943] (II) VIVANTE(0): test Initializing EXA

[ 83014.943] (II) VIVANTE(0): (driver build from: -dirty)

[ 83014.950] (II) EXA(0): Driver allocated offscreen pixmaps

[ 83014.950] (II) EXA(0): Driver registered support for the following operations:

[ 83014.950] (II)         Solid

[ 83014.951] (II)         Copy

[ 83014.951] (II)         Composite (RENDER acceleration)

[ 83014.951] (II)         UploadToScreen

[ 83014.980] (II) VIVANTE(0): Init SHM pixmap support

[ 83014.981] (==) VIVANTE(0): Backing store enabled

[ 83014.986] (==) VIVANTE(0): DPMS enabled

[ 83014.986] (II) VIVANTE(0): RandR 1.2 enabled, ignore the following RandR disabled message.

[ 83014.988] drmOpenDevice: node name is /dev/dri/card0

[ 83014.988] drmOpenDevice: open result is 10, (OK)

[ 83014.988] drmOpenDevice: node name is /dev/dri/card0

[ 83014.988] drmOpenDevice: open result is 10, (OK)

[ 83014.988] drmOpenByBusid: Searching for BusID platform:Vivante GCCore:00

[ 83014.988] drmOpenDevice: node name is /dev/dri/card0

[ 83014.988] drmOpenDevice: open result is 10, (OK)

[ 83014.988] drmOpenByBusid: drmOpenMinor returns 10

[ 83014.988] drmOpenByBusid: drmGetBusid reports platform:Vivante GCCore:00

[ 83014.988] (II) [drm] DRM interface version 1.4

[ 83014.989] (II) [drm] DRM open master succeeded.

[ 83014.989] (II) VIVANTE(0): [drm] Using the DRM lock SAREA also for drawables.

[ 83014.989] (II) VIVANTE(0): [drm] framebuffer handle = 0x48900000

[ 83014.989] (II) VIVANTE(0): [drm] added 1 reserved context for kernel

[ 83014.989] (II) VIVANTE(0): X context handle = 0x1

[ 83014.989] (II) VIVANTE(0): [drm] installed DRM signal handler

[ 83014.989] (II) VIVANTE(0): [DRI] installation complete

[ 83014.989] (--) RandR disabled

[ 83015.029] (II) AIGLX: Screen 0 is not DRI2 capable

[ 83015.029] (EE) AIGLX: reverting to software rendering

[ 83015.153] (II) AIGLX: Loaded and initialized swrast

[ 83015.154] (II) GLX: Initialized DRISWRAST GL provider for screen 0

[ 83015.157] (II) VIVANTE(0): Setting screen physical size to 508 x 285

[ 83015.382] (II) config/udev: Adding input device Logitech USB Optical Mouse (/dev/input/event1)

[ 83015.382] (**) Logitech USB Optical Mouse: Applying InputClass "evdev pointer catchall"

[ 83015.382] (II) LoadModule: "evdev"

[ 83015.382] (II) Loading /usr/lib/xorg/modules/input/evdev_drv.so

[ 83015.393] (II) Module evdev: vendor="X.Org Foundation"

[ 83015.393]    compiled for 1.16.3, module version = 2.9.1

[ 83015.393]    Module class: X.Org XInput Driver

[ 83015.393]    ABI class: X.Org XInput driver, version 21.0

[ 83015.393] (II) Using input driver 'evdev' for 'Logitech USB Optical Mouse'

[ 83015.393] (**) Logitech USB Optical Mouse: always reports core events

[ 83015.393] (**) evdev: Logitech USB Optical Mouse: Device: "/dev/input/event1"

[ 83015.394] (--) evdev: Logitech USB Optical Mouse: Vendor 0x46d Product 0xc05a

[ 83015.394] (--) evdev: Logitech USB Optical Mouse: Found 3 mouse buttons

[ 83015.394] (--) evdev: Logitech USB Optical Mouse: Found scroll wheel(s)

[ 83015.394] (--) evdev: Logitech USB Optical Mouse: Found relative axes

[ 83015.394] (--) evdev: Logitech USB Optical Mouse: Found x and y relative axes

[ 83015.394] (II) evdev: Logitech USB Optical Mouse: Configuring as mouse

[ 83015.394] (II) evdev: Logitech USB Optical Mouse: Adding scrollwheel support

[ 83015.394] (**) evdev: Logitech USB Optical Mouse: YAxisMapping: buttons 4 and 5

[ 83015.394] (**) evdev: Logitech USB Optical Mouse: EmulateWheelButton: 4, EmulateWheelInertia: 10, EmulateWheelTimeout: 200

[ 83015.394] (**) Option "config_info" "udev:/sys/devices/soc0/soc.0/2100000.aips-bus/2184200.usb/ci_hdrc.1/usb1/1-1/1-1.1/1-1.1:1.0/0003:046D:C05A.0001/input/input1/event1"

[ 83015.394] (II) XINPUT: Adding extended input device "Logitech USB Optical Mouse" (type: MOUSE, id 6)

[ 83015.394] (II) evdev: Logitech USB Optical Mouse: initialized for relative axes.

[ 83015.395] (**) Logitech USB Optical Mouse: (accel) keeping acceleration scheme 1

[ 83015.395] (**) Logitech USB Optical Mouse: (accel) acceleration profile 0

[ 83015.395] (**) Logitech USB Optical Mouse: (accel) acceleration factor: 2.000

[ 83015.395] (**) Logitech USB Optical Mouse: (accel) acceleration threshold: 4

[ 83015.397] (II) config/udev: Adding input device Logitech USB Optical Mouse (/dev/input/mouse1)

[ 83015.398] (II) No input driver specified, ignoring this device.

[ 83015.398] (II) This device may have been added with another device file.

[ 83015.400] (II) config/udev: Adding input device Logitech USB Keyboard (/dev/input/event2)

[ 83015.400] (**) Logitech USB Keyboard: Applying InputClass "evdev keyboard catchall"

[ 83015.400] (II) Using input driver 'evdev' for 'Logitech USB Keyboard'

[ 83015.400] (**) Logitech USB Keyboard: always reports core events

[ 83015.400] (**) evdev: Logitech USB Keyboard: Device: "/dev/input/event2"

[ 83015.400] (--) evdev: Logitech USB Keyboard: Vendor 0x46d Product 0xc31c

[ 83015.400] (--) evdev: Logitech USB Keyboard: Found keys

[ 83015.400] (II) evdev: Logitech USB Keyboard: Configuring as keyboard

[ 83015.400] (**) Option "config_info" "udev:/sys/devices/soc0/soc.0/2100000.aips-bus/2184200.usb/ci_hdrc.1/usb1/1-1/1-1.2/1-1.2:1.0/0003:046D:C31C.0002/input/input2/event2"

[ 83015.400] (II) XINPUT: Adding extended input device "Logitech USB Keyboard" (type: KEYBOARD, id 7)

[ 83015.400] (**) Option "xkb_rules" "evdev"

[ 83015.400] (**) Option "xkb_model" "pc104"

[ 83015.400] (**) Option "xkb_layout" "us"

[ 83015.514] (II) config/udev: Adding input device Logitech USB Keyboard (/dev/input/event3)

[ 83015.514] (**) Logitech USB Keyboard: Applying InputClass "evdev keyboard catchall"

[ 83015.514] (II) Using input driver 'evdev' for 'Logitech USB Keyboard'

[ 83015.514] (**) Logitech USB Keyboard: always reports core events

[ 83015.514] (**) evdev: Logitech USB Keyboard: Device: "/dev/input/event3"

[ 83015.515] (--) evdev: Logitech USB Keyboard: Vendor 0x46d Product 0xc31c

[ 83015.515] (--) evdev: Logitech USB Keyboard: Found absolute axes

[ 83015.515] (II) evdev: Logitech USB Keyboard: Forcing absolute x/y axes to exist.

[ 83015.515] (--) evdev: Logitech USB Keyboard: Found keys

[ 83015.515] (II) evdev: Logitech USB Keyboard: Forcing relative x/y axes to exist.

[ 83015.515] (II) evdev: Logitech USB Keyboard: Configuring as mouse

[ 83015.515] (II) evdev: Logitech USB Keyboard: Configuring as keyboard

[ 83015.515] (**) Option "config_info" "udev:/sys/devices/soc0/soc.0/2100000.aips-bus/2184200.usb/ci_hdrc.1/usb1/1-1/1-1.2/1-1.2:1.1/0003:046D:C31C.0003/input/input3/event3"

[ 83015.515] (II) XINPUT: Adding extended input device "Logitech USB Keyboard" (type: KEYBOARD, id 8)

[ 83015.515] (**) Option "xkb_rules" "evdev"

[ 83015.515] (**) Option "xkb_model" "pc104"

[ 83015.515] (**) Option "xkb_layout" "us"

[ 83015.516] (II) evdev: Logitech USB Keyboard: initialized for absolute axes.

[ 83015.516] (**) Logitech USB Keyboard: (accel) keeping acceleration scheme 1

[ 83015.516] (**) Logitech USB Keyboard: (accel) acceleration profile 0

[ 83015.517] (**) Logitech USB Keyboard: (accel) acceleration factor: 2.000

[ 83015.517] (**) Logitech USB Keyboard: (accel) acceleration threshold: 4

[ 83015.518] (II) config/udev: Adding input device max11801_ts (/dev/input/event0)

[ 83015.518] (**) max11801_ts: Applying InputClass "evdev touchscreen catchall"

[ 83015.518] (II) Using input driver 'evdev' for 'max11801_ts'

[ 83015.518] (**) max11801_ts: always reports core events

[ 83015.519] (**) evdev: max11801_ts: Device: "/dev/input/event0"

[ 83015.519] (--) evdev: max11801_ts: Vendor 0 Product 0

[ 83015.519] (--) evdev: max11801_ts: Found absolute axes

[ 83015.519] (--) evdev: max11801_ts: Found x and y absolute axes

[ 83015.519] (--) evdev: max11801_ts: Found absolute touchscreen

[ 83015.519] (II) evdev: max11801_ts: Configuring as touchscreen

[ 83015.519] (**) evdev: max11801_ts: YAxisMapping: buttons 4 and 5

[ 83015.519] (**) evdev: max11801_ts: EmulateWheelButton: 4, EmulateWheelInertia: 10, EmulateWheelTimeout: 200

[ 83015.519] (**) Option "config_info" "udev:/sys/devices/soc0/soc.0/2100000.aips-bus/21a0000.i2c/i2c-0/0-0048/input/input0/event0"

[ 83015.519] (II) XINPUT: Adding extended input device "max11801_ts" (type: TOUCHSCREEN, id 9)

[ 83015.519] (II) evdev: max11801_ts: initialized for absolute axes.

[ 83015.520] (**) max11801_ts: (accel) keeping acceleration scheme 1

[ 83015.520] (**) max11801_ts: (accel) acceleration profile 0

[ 83015.520] (**) max11801_ts: (accel) acceleration factor: 2.000

[ 83015.520] (**) max11801_ts: (accel) acceleration threshold: 4

[ 83015.521] (II) config/udev: Adding input device max11801_ts (/dev/input/mouse0)

[ 83015.521] (II) No input driver specified, ignoring this device.

[ 83015.521] (II) This device may have been added with another device file.

标签 (4)
0 项奖励
回复
1 解答
4,832 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Mirko

please use sect.5.6.6 Chromium Browser on X11, XWayland and Wayland

attached Yocto User Guide and L4.1.15_1.0.0_MX6QDPSABRESD (REV L4.1.15_1.0.0)

Board Support Packages (35)

L4.1.15_1.0.0_MX6QDLSOLO (REV L4.1.15_1.0.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
4,833 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Mirko

please use sect.5.6.6 Chromium Browser on X11, XWayland and Wayland

attached Yocto User Guide and L4.1.15_1.0.0_MX6QDPSABRESD (REV L4.1.15_1.0.0)

Board Support Packages (35)

L4.1.15_1.0.0_MX6QDLSOLO (REV L4.1.15_1.0.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
4,832 次查看
mirkoardinghi1
Contributor IV

I have followed the instruction but the problem remains.

[998:998:0412/124522:ERROR:gl_surface_glx.cc(637)] glXChooseFBConfig failed.

[998:998:0412/124522:ERROR:gpu_info_collector.cc(27)] gfx::GLContext::CreateOffscreenGLSurface failed

[998:998:0412/124522:ERROR:gpu_info_collector.cc(89)] Could not create surface for info collection.

[998:998:0412/124522:ERROR:gpu_main.cc(421)] gpu::CollectGraphicsInfo failed (fatal).

[998:998:0412/124522:ERROR:gpu_child_thread.cc(145)] Exiting GPU process due to errors during initialization

Perform final cleanup before process termination!

0 项奖励
回复
4,832 次查看
mirkoardinghi1
Contributor IV

It works!

Thanks

0 项奖励
回复