Chromium browser does not start in user context

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Chromium browser does not start in user context

4,298件の閲覧回数
MicMoba
Contributor V

I want to use Chromium-ozone-wayland browser on my device. I had build the yocto image sucessfully. Chrome Version: Chromium 96.0.4664.110 stable

When I start chromium as user I got the following error message:

 

user@ ~$ chromium 
[1223:1223:0222/143357.967200:ERROR:process_singleton_posix.cc(340)] Failed to create /home/moba/.config/chromium/SingletonLock: Operation not permitted (1)
[1223:1223:0222/143357.967678:ERROR:chrome_browser_main.cc(1313)] Failed to create a ProcessSingleton for your profile directory. This means that running multiple instances would start multiple browser processes rather than opening a new window in the existing process. Aborting now to avoid profile corruption.

 

 I can start chromium as root user with 'chromium --no-sandbox'

What does it mean 'Failed to create a ProcessSingleton'? My home is located on a fat32 partition. But I can not image that this has something to do with it.

 

Edit:

When I use 'chromium --user-data-dir=/tmp/' chromium started. So error maybe depends on the fat32 partition?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

4,258件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

looking through the web this seems to be a problem related to the space left in your partition:
https://bugs.chromium.org/p/chromium/issues/detail?id=73035
https://stackoverflow.com/questions/38894321/chromium-browser-singleton-bug-caused-by-power-failure

Best regards,
Aldo.

0 件の賞賛
返信

4,253件の閲覧回数
MicMoba
Contributor V

Hi AldoG,

thanks for the hints. I checked the remaining space at my home directory. It is over 5GB free space available. But it is a FAT32 partition. The rootfs is an ext4 partition. Maybe it has something to do with the mixture of both filesystems.

0 件の賞賛
返信