Chenge to USB PHY Receiver Control Register

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Chenge to USB PHY Receiver Control Register

1,481 Views
takashitakahash
Contributor III

Hi community.

Our customer has question below.

About USB PHY Receiver Control Register of (USBPHYx_RXn) for "DISCONADJ"

Customer want to chenge to  initial value from 000 (575mV) from set change in 011 (587.5mV).

Would you please advice of concern point set to DISCONADJ = 011(587.5mV).

[ Background of the question ]

Customer would like to set USB PHY Transmitter Control Register of (USBPHYx_TXn) the "D_CAL" to 011 for EYE pattern quality impruvement.,

It would detect problems Disconnection in combination with a specific device has occurred in its influence.

However, in order to be avoided problems by increasing the threshold of detection Disconnect from 575mV to 587.5mV, we have to consider the configuration changes.

Thanks,

Best.

Labels (1)
0 Kudos
Reply
3 Replies

1,234 Views
art
NXP Employee
NXP Employee

To make me able to provide you with an accurate answer, please first specify what exactly i.MX family processor do you mean. Is it some of i.MX6 series family? If so, please specify what exacly i.MX6 processor (Quad, Dual, DualLite, Solo, SoloLite, SoloX, UltraLite) do you use.

Best Regards,

Artur

0 Kudos
Reply

1,234 Views
takashitakahash
Contributor III

Dear Artur

Thank you for your replay.

Customer use i.MX6DualLite.

Best Regards,

T.Takahashi

0 Kudos
Reply

1,234 Views
takashitakahash
Contributor III

Dear Artur-san.

I  have Additional questions.

To Disconnect detection voltage Will there is variation. (Temperature characteristic)

If there is a temperature variation , Would  like to how much of the variation .(precision).

Thank you,

Best Regards.

T.Takahahsi

0 Kudos
Reply