Changing kernel start address

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Changing kernel start address

1,820 次查看
dogisfat
Contributor IV

I have implemented the change detailed in Application note AN5127 (https://www.nxp.com/docs/en/application-note/AN5127.pdf) successfully for a i.MX7D platform with kernel 4.9. I am trying to update to a Yocto Kirkstone based BSP with kernel 5.10 and am failing to successfully boot when making the same modifications. The system gets stuck after printing "Staring Kernel ..." 

What changes should I be aware of that will require additional changes to the kernel to get the modifications working for Kernel 5.10?

标签 (1)
0 项奖励
回复
3 回复数

1,676 次查看
dogisfat
Contributor IV

I have narrowed the failure to boot to be in the __turn_mmu_on function in arch/arm/kernel/head.S. Unfortunately the comment for __turn_mmu_on specifies that you cannot trace through this function which I assume applies to jtag debuggers. I also have been unable to print to the UART though it (unsurprisingly).

What do I need to verify prior to that call to ensure the platform is correctly set up?

0 项奖励
回复

1,782 次查看
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

If it fails when specifying the kernel address, what happen if you don't and flash a fresh build?

Regards

0 项奖励
回复

1,778 次查看
dogisfat
Contributor IV

If the modifications detailed in the application note are not implemented the kernel boots and functions normally.

0 项奖励
回复