Changing SCU UART Pins

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Changing SCU UART Pins

1,542件の閲覧回数
MJames
Contributor I

Hi,

I am using a custom board with iMX8QXP. For debug purposes, I had to change the SCU UART pins to the M4 UART pins. I did the following change in the board.c file according to the document:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Use-UART0-RX-TX-as-SCU-UART-debug-port-o...

#define ALT_DEBUG_UART and #define ALT_DEBUG_SCU_UART. I added these to the board.c file. It worked and I was able to get prints from the SCU on the M4 core console.

The initial SCU UART pins used are:

       SCU_GPIO0_00 & SCU_GPIO0_01

The M4 UART pins used are:

       ADC_IN2 & ADC_IN3

I would like to revert to the previous settings. I removed the above change and rebuilt the SCFW. But now I am getting SCU prints on both the M4 console and on the original SCU UART pins. I even tried re-flashing the board with a firmware, built from a fresh source code. But still no change. How can I fix this?

@qiang_li-mpu_se Could you please look into this?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,526件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Please make sure that all changes made are reverted.
Also, you may try using a fresh source code instead.

Saludos,
Aldo

0 件の賞賛
返信

1,511件の閲覧回数
MJames
Contributor I

Hi @AldoG,
I have tried after reverting all the changes, but the issue is not resolved. I have also tried changing the entire firmware, built from a fresh source code. Still there is no change.

0 件の賞賛
返信