Change eMMC operating mode to HS200

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Change eMMC operating mode to HS200

4,255件の閲覧回数
nirmalluhana
Contributor IV

Hello,

 

Release: Yocto-Sumo (4.14.78_1.0.0_GA)

Board: i.MX8MQ based custom board

We designed iMX8MQ based custom board and used eMMC as booting option.

Right now, our eMMC is operated in HS400 mode as mentioned in kernel debug logs.

root@imx8mqpicoitx:~# cat /sys/kernel/debug/mmc0/ios
clock:          200000000 Hz
actual clock:   200000000 Hz
vdd:            21 (3.3 ~ 3.4 V)
bus mode:       2 (push-pull)
chip select:    0 (don't care)
power mode:     2 (on)
bus width:      3 (8 bits)
timing spec:    10 (mmc HS400)
signal voltage: 1 (1.80 V)
driver type:    0 (driver type B)
root@imx8mqpicoitx:~#

We want to change eMMC operating mode to HS200.

So, for that which changes we have to change in dts file or in eMMC driver source?

Best regards,

Nirmal

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

3,758件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Nirmal,

The following thread may be of help:

https://community.nxp.com/thread/494187 

Regards,

0 件の賞賛
返信