Change eMMC operating mode to HS200

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Change eMMC operating mode to HS200

4,283 次查看
nirmalluhana
Contributor IV

Hello,

 

Release: Yocto-Sumo (4.14.78_1.0.0_GA)

Board: i.MX8MQ based custom board

We designed iMX8MQ based custom board and used eMMC as booting option.

Right now, our eMMC is operated in HS400 mode as mentioned in kernel debug logs.

root@imx8mqpicoitx:~# cat /sys/kernel/debug/mmc0/ios
clock:          200000000 Hz
actual clock:   200000000 Hz
vdd:            21 (3.3 ~ 3.4 V)
bus mode:       2 (push-pull)
chip select:    0 (don't care)
power mode:     2 (on)
bus width:      3 (8 bits)
timing spec:    10 (mmc HS400)
signal voltage: 1 (1.80 V)
driver type:    0 (driver type B)
root@imx8mqpicoitx:~#

We want to change eMMC operating mode to HS200.

So, for that which changes we have to change in dts file or in eMMC driver source?

Best regards,

Nirmal

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

3,786 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Nirmal,

The following thread may be of help:

https://community.nxp.com/thread/494187 

Regards,

0 项奖励
回复