Case:00092377: gpu renderiing using Adobe Air application apk in MCIMX6Q-SDP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Case:00092377: gpu renderiing using Adobe Air application apk in MCIMX6Q-SDP

3,247 次查看
ryang
Contributor III

Case:00092377: gpu renderiing using Adobe Air application apk in MCIMX6Q-SDP

Board name: MCIMX6Q-SDP

Andriod: M6.0.1_2.0.0

Subject: gpu rendering using adobe Air application APK and picture attached.

请先将runState.txt和floorInfo.txt放在 /sdcard/Parameter2里面,然后安装adobe air环境AdobeAIR.apk,再安装打开D1_1024_2.2.apk即可看到画面

Original Attachment has been moved to: D1_1024_2.2.apk.zip

Original Attachment has been moved to: AdobeAIR.apk.zip

标签 (1)
0 项奖励
回复
2 回复数

3,110 次查看
ryang
Contributor III

running=1&direction=2&currentFloor=25&currentMode=0&nextStopFloors=3,2,4&DFKR=0&scrollInterval=9

<root>
 <floor display="B1">
  <picURL>file://C:/Users/test/Parameter2/floorPics/b1.png</picURL>
 </floor>
 <floor display="1">
  <picURL>file://C:/Users/test/Parameter2/floorPics/1.png</picURL>
 </floor>
 <floor display="2">
  <picURL>file://C:/Users/test/Parameter2/floorPics/2.png</picURL>
 </floor>

</root>

0 项奖励
回复

3,110 次查看
igorpadykov
NXP Employee
NXP Employee

Hello rita

unfortunately I am not aware of Adobe Air use cases with i.MX6, for that

reason may be recommended to apply to MSS services for

help with integration Adobe freamework with i.MX6 Android.

Best regards
igor

0 项奖励
回复