Capture raw format(yuv420)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Capture raw format(yuv420)

1,831 Views
erikraynolds
Contributor IV

Dears

I need to have camera capture of raw format. I'm using I. Mx6. I have mipi csi camera capable of 30fps. Can I get video recording of 30fps and so how / what sw to use? 

I'm not looking for to use compression and really look for raw format capturing at max FPS. 

Thanks 

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,544 Views
igorpadykov
NXP Employee
NXP Employee

Hi Erik

raw format is not supported in nxp official bsps.

There are some posts covering some topics about raw capture

https://community.nxp.com/thread/302769

https://community.nxp.com/thread/320618

CSI -> IPU -> MEM retrieve 16 bits RAW DATA 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply