Cany imx6q support paralle raw data?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cany imx6q support paralle raw data?

2,371 Views
fangduoxu
Contributor I

Dear NXP ,

I have a question. Can imx6q support raw data (8bit) with parallel interface?  I have an raw data camera connected to imx6q with parallel interface. I am not sure if this connection can get raw data correctly. By the way , do you have raw data relaged patches for imx6q?

Thanks.

Labels (1)
0 Kudos
Reply
4 Replies

2,180 Views
fangduoxu
Contributor I

I have read almost all discussions here related to raw or bayer . Some of them are MIPI interface for raw data output, others are not clear if they are successfull in getting raw data through parallel interface. 

Most of the solutions are following IPU_PIX_FMT_GENERIC to add IPU_PIX_FMT_GREY.  I have tested these changes mentioned in these discussions, but still not sure if these patches are full or useful.  

Can anyone provide a full and clear patch for raw data sensor with parallel interface? My board is i.MX6Q.

  

Thanks .

0 Kudos
Reply

2,180 Views
joanxie
NXP TechSupport
NXP TechSupport

yes, the set is correct, if you need to use 8BITS, first you need to ensure you connect successfully correctly on hardware, we just patch for bt565 8bits, for raw data, one can set as you mentioned, if you have further questions, you can post your issue

0 Kudos
Reply

2,180 Views
fangduoxu
Contributor I

Thank you for your reply.

Where can I get related patch(or patches) to support raw data (8bit) sensor with parallel interface(DVP, not MIPI )? 

I am new to iMX 6 and other iMX SOCs. Please help.

0 Kudos
Reply

2,180 Views
joanxie
NXP TechSupport
NXP TechSupport

yes, mx6q can support this.

0 Kudos
Reply