Cannot decode h.264 streams on i.MX51

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cannot decode h.264 streams on i.MX51

1,588件の閲覧回数
StephanHaller
Contributor I
Hi, I have a problem decoding h.264 streams on i.MX51. I get the stream demuxed by ffmpeg so that my class handles only the video data. It works good for mpeg2 and mpeg4 streams but not on h.264 streams. The problem is at the very beginning of decoding: vpu_DecGetInitialInfo(,.) returns failure. It also puts the reason code 1 in the structure DecInitialInfo. ---- RetCode error; DecInitialInfo initialInfo={0}; vpu_DecSetEscSeqInit(m_decoder.handle, 1); error=vpu_DecGetInitialInfo(m_decoder.handle, &initialInfo); vpu_DecSetEscSeqInit(m_decoder.handle, 0); if(error!=RETCODE_SUCCESS) { printf("Failed to get initial info of vpu_DecGetInitialInfo - return code %d, reason code %d\n", error, initialInfo.errorcode); return ERROR; } ---- You will get "Failed to get initial info of vpu_DecGetInitialInfo - return code -1, error code 1". So what is reason code in this structure? Is there any table describing the reason codes? I use VPU firmware version 1.4.14 and library version 5.3.2. Thanks for any help Stephan Haller
タグ(2)
0 件の賞賛
返信
1 返信

1,407件の閲覧回数
stevejhung
Contributor I

I am having a similar problem with my imx515. Stream decodes but is out of sync. I'm guessing it's somewhere in the code that deals with timestamp, but haven't had a chance to trace it down though.

Steve

0 件の賞賛
返信