Can we interface MT25QL02GCBB8E12-0SIT in QSPI mode with i.MX6 Quad or not?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can we interface MT25QL02GCBB8E12-0SIT in QSPI mode with i.MX6 Quad or not?

723 次查看
sagar_kumar
Contributor I

Hi

Can we interface XIP NOR FLASH MT25QL02GCBB8E12-0SIT (2Gb- 256Mx8) in QSPI mode with i.MX6 Quad or not?

标签 (1)
0 项奖励
回复
1 回复

661 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sagar

i.MX6Q does not support boot from qspi nor, supported boot devives are described in

Chapter 8 System Boot i.MX6DQ Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复