Can we interface MT25QL02GCBB8E12-0SIT in QSPI mode with i.MX6 Quad or not?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can we interface MT25QL02GCBB8E12-0SIT in QSPI mode with i.MX6 Quad or not?

698件の閲覧回数
sagar_kumar
Contributor I

Hi

Can we interface XIP NOR FLASH MT25QL02GCBB8E12-0SIT (2Gb- 256Mx8) in QSPI mode with i.MX6 Quad or not?

ラベル(1)
0 件の賞賛
返信
1 返信

636件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sagar

i.MX6Q does not support boot from qspi nor, supported boot devives are described in

Chapter 8 System Boot i.MX6DQ Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信