Can't get wlan0 interface up while using murata on linux-rel_imx_4.9.x_1.0.0_ga

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can't get wlan0 interface up while using murata on linux-rel_imx_4.9.x_1.0.0_ga

1,856 次查看
jeangardyvalent
Contributor II

Hi guys,

I'm working an imx6ull board and murata device type 1DX  and i have some issues while using nxp linux release rel_imx_4.9.x_1.0.0_ga.

First of all i have tested the murata on linux version rel_imx_4.1.15_2.0.0 and everything was working fine. I upated the linux version to 4.9.x and the murata firmware also by downloading the correct one (4.9.11) on NXP website. The bcmdhd driver has been initialized correctly and i have issue with "HT clock" while trying to use wpa_supplicant to apply settings on wlan0 and to put it up by using this command :

      wpa_supplicant -i wlan0 -Dnl80211 -c /etc/wpa_supplicant.conf -B&

I have attached all log files.

Issue log :

  dhdsdio_htclk: HT Avail timeout (1000000): clkctl 0x50
dhdsdio_htclk: HT Avail timeout (1000000): clkctl 0x50
dhdsdio_htclk: HT Avail timeout (1000000): clkctl 0x50
dhdsdio_htclk: HT Avail request error: retried 20 times. UNRECOVERABLE!
dhd_net_bus_devreset: dhd_bus_devreset: -1
dhd_open : wl_android_wifi_on failed (-1)
wl_android_wifi_off in
dhd_prot_ioctl : bus is down. we have nothing to do
dhd_net_bus_devreset: dhd_bus_devreset: -35
Could not set interface wlan0 flags (UP): Operation not permitted
nl80211: Could not set interface 'wlan0' UP
nl80211: deinit ifname=wlan0 disabled_11b_rates=0
wlan0: Failed to initialize driver interface

Is somebody has an idea?

Best regards

Jean Gardy

标记 (1)
0 项奖励
回复
1 回复

1,488 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi Jean,

in this case the problem will be the Murata drivers, so you may contact Murata to get the appropriate drivers.


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复