Can't download linux code 3.14.28

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't download linux code 3.14.28

1,039件の閲覧回数
mingmingyuan
Contributor III

download repo output error infomation as blow:

ymm@ymm:~$ curl http://commondatastorage.googleapis.com/git-repo-downloads/repo > ~/bin/repo

  % Total    % Received % Xferd  Average Speed   Time    Time     Time  Current

                                 Dload  Upload   Total   Spent    Left  Speed

  0     0    0     0    0     0      0      0 --:--:--  0:02:07 --:--:--     0curl: (7) Failed to connect to 2404:6800:4005:80a::2001: 网络不可达

ラベル(2)
0 件の賞賛
返信
1 返信

983件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Mingming Yuan,

Are you still experiencing this issue? I would recommend that you make sure you have access to the internet, especially if a proxy needs to be configured.

0 件の賞賛
返信