Can't build Android Things images

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't build Android Things images

ソリューションへジャンプ
2,336件の閲覧回数
stefanosanna
Contributor I

Following the instructions in the PICO-i MX6UL-QSG.pdf document, I'm not able to self-build the Android Things images for the PICO board. More precisely, the command "lunch iot_imx6ul_pico-eng" fails because the "iot_imx6ul_pico-eng" configuration does not exist. Probably it needs a different bootloader, I was unable to find it. Where may I find update information on this topic?

Thank you.

Stefano.

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 解決策
1,879件の閲覧回数
robertthompsons
NXP Employee
NXP Employee

Do to a last minute change by Google the source for Android Things will not be pushed to the AOSP until code is production ready. Based on this currently only the binary image is available from System Image Downloads | Android Things 

The updated docs can be found at: Android Things with i.MX 6UL|NXP 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,880件の閲覧回数
robertthompsons
NXP Employee
NXP Employee

Do to a last minute change by Google the source for Android Things will not be pushed to the AOSP until code is production ready. Based on this currently only the binary image is available from System Image Downloads | Android Things 

The updated docs can be found at: Android Things with i.MX 6UL|NXP 

0 件の賞賛
返信