Can someone point me to the cpu temperature sensor calibration procedure on the iMX6 device?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can someone point me to the cpu temperature sensor calibration procedure on the iMX6 device?

2,212 Views
philipchapman
Contributor I

Hello,

I need the procedure to calibrate the iMX6 internal temperature sensor.

can someone point me to the process

Thanks

0 Kudos
Reply
5 Replies

1,687 Views
kshitij_shah
NXP Employee
NXP Employee

Hi Igor,

If you know someone who has more information, please provide the contact details.

Also "5.4.1.4 Local temperature sensor placement" has two tables with list of sensors, which one is correct?

0 Kudos
Reply

1,687 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kshitij

 

please create new thread for questions related to i.MX8M processor, as

this thread was for i.MX6.

Regarding i.MX8M, unfortunately I am not aware who has more information,

in general you can get more info in local nxp marketing office.

Best regards
igor

0 Kudos
Reply

1,687 Views
kshitij_shah
NXP Employee
NXP Employee

Hi Igor,

Can you please point to documentation for process to do sensor calibration on iMX8M ?

Thanks

0 Kudos
Reply

1,687 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kshitij

one can look on sect.5.4.2.18 TMU Temperature Range n Control register (TMU_TTRnCR)

i.MX8MDQ Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMX8MDQLQRM.pdf

I am not aware of additional documentation on that subject.

Best regards
igor

0 Kudos
Reply

1,687 Views
igorpadykov
NXP Employee
NXP Employee

Hi Philip

please check AN5215 i.MX6 Temperature Sensor Module
http://www.nxp.com/docs/en/application-note/AN5215.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply