Can Serial Downloader be triggered from uboot/userspace?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can Serial Downloader be triggered from uboot/userspace?

2,723 Views
dav1
Contributor V

Is it possible (on the i.mx8 mini) to override the BOOT_MODE pins (via code/register write) to enable the Serial Downloader (without having to physically change the boot-pins)

0 Kudos
Reply
4 Replies

2,516 Views
art
NXP Employee
NXP Employee

No, it is not possible to override the BOOT_MODE[1:0] settings in software without physically switching the BOOT_MODE[1:0] pins.

Best Regards,

Artur

0 Kudos
Reply

2,516 Views
dav1
Contributor V

Hi Artur,

iMX7's u-boot's bmode usb command writes to gpr9 and gpr10 (general purpose registers). The same register on the imx8m mini's reference manual states these are "reserved for internal use"...

Can you please check with the i.mx8 team if these still exists but are not documented.

0 Kudos
Reply

2,516 Views
art
NXP Employee
NXP Employee

The R&D have confirmed that there is no way to override the boot mode settings in software.

0 Kudos
Reply

2,516 Views
dav1
Contributor V

FYI: fastboot can be used to override say emmc boot and instead jump into the serial-downloader mode.

0 Kudos
Reply