Hey there,
I have a set-up that is running a i.MX 8QuadMax CPU on top of the MCIMX8-8X-BB base board. I saw that there are two audio slots. So I ask myself:
Thanks much and have a great day!
Solved! Go to Solution.
1. No, the current BSP release is prepared to work only with one IMX-AUD-IO board.
2. Unfortunately it is not documented or tested, just one card.
3. No, it is for sale together with the base board only.
4. Are you referring to this jumper?
Thanks for the clarification.
Yes, I am referring to this jumper. Is this basically a selection if audio gets routed to IMX-AUD-IO slot 1 or 2 or is there more logic to it?
Also from the hardware perspective: Would it even be possible to route different audio signals to two different IMX-AUD-IO boards (in case the BSP would support it)?
J47 it is used to select the board that is connected to base board:
- Rev D MCIMX8QXP-CPU - NA.
- Rev C MCIMX8QXP-CPU - Short Pins 1 & 2.
- MCIMX8QM-CPU - Short Pins 2 & 3.
And H4 jumper selects the use of audio slot 1, short the pins of H4 with a Jumper while connecting the LCD Card in Audio slot 1.
> Also from the hardware perspective: Would it even be possible to route different audio signals to two different IMX-AUD-IO boards (in case the BSP would support it)?
Yes, it is correct, audio slot 1 use ESAI0 while audio slot 2 use ESAI1, but it is not implemented on current BSP release.
1. No, the current BSP release is prepared to work only with one IMX-AUD-IO board.
2. Unfortunately it is not documented or tested, just one card.
3. No, it is for sale together with the base board only.
4. Are you referring to this jumper?