Can I use Codewarrior as a Linux Kernel Debugger for the MCIMX8M-EVK?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I use Codewarrior as a Linux Kernel Debugger for the MCIMX8M-EVK?

1,412 Views
mindchasers
Contributor III

Hello,

We have Codewarrior experience on QorIQ/Layerscape devices and some NXP Codewarrior JTAG TAP boxes. 

Can Codewarrior be used to debug the Linux Kernel on the i.MX8MQ? 

We're currently evaluating ARM's DS solution with our  MCIMX8M-EVK development board, but we have an interest to stick with CodeWarrior. 

Thank you,

Bob

0 Kudos
Reply
1 Reply

1,346 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Robert,

>>Can Codewarrior be used to debug the Linux Kernel on the i.MX8MQ? 

No, Codewarrior can't be used to debug i.MX processors.

>>We're currently evaluating ARM's DS solution with our  MCIMX8M-EVK development board

ARM DS5 is OK. If you want to debug M4 core in i.MX8MQ, Jlink Plus can be used.

Hope above information is helpful for you.

Have a nice day!

BR,

Weidong

0 Kudos
Reply