Can I set a specific pixel to a RGB value?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I set a specific pixel to a RGB value?

1,751 Views
scottwalter
Contributor I

Hey guys,

I'm developing an HDMI driver for the i.IMX6 board. This is my first time writing a driver so I'm a little new to this. I was looking for two specific features present in the HDMI configuration registers that I can't seem to find:

1. Can you set a specific pixel to be a certain RGB value?

- In the SDK code for the HDMI there's a nice way to force the entire screen to be one color but not an individual pixel.

2. Is there a way to disable/enable the backlight, turn on/off the screen via the HDMI config registers? Based on previous i.MX boards this was done by altering one simple register. Is it the same for i.MX6?

Thanks!

Labels (1)
Tags (3)
0 Kudos
Reply
2 Replies

1,655 Views
joanxie
NXP TechSupport
NXP TechSupport

1. Can you set a specific pixel to be a certain RGB value?

> what specific pixel do you need to set? pls give me detailed case for check

2. Is there a way to disable/enable the backlight, turn on/off the screen via the HDMI config registers?

> via HDMI config register? no, hdmi config register couldn't control backlight. you can refer to the "imx6q_add_mxc_pwm_backlight" fucntion in the "arch\am\mach-mx6\board-m6q_sabresd.c". imx products have the familiar PWM module.

0 Kudos
Reply

1,655 Views
scottwalter
Contributor I

what specific pixel do you need to set? pls give me detailed case for check

> For instance, I want to set pixel 250,59 to the RGB value 35,20,16 (totally random).

0 Kudos
Reply