Can I do not supply power for PCIE-HDMI-SATA-USB if not use them?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can I do not supply power for PCIE-HDMI-SATA-USB if not use them?

826 次查看
翔李
Contributor IV

HI,

If I don't use PCIE,SATA,HDMI,USB OF IMX6Q-IMX6 DUAL-SOLO etc,is it necessary to supply the power of their VCC-IN PIN? Can I NC these following PINS?
SATA_VP_VPH,,,HDMI_VP_VPH,,,PCIE_VP_VPH_VPTX,,,USB_VBUS.

What is more,If I don't use USB,Can I do not stuff 24MHZ CRYSTAL?

pastedImage_1.png

pastedImage_2.png

pastedImage_3.png

pastedImage_4.png

0 项奖励
回复
2 回复数

695 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,

  For PCIE,SATA & HDMI, if you don't use them, not necessary to supply them, so you can make corresponding resistors NC.

  But for USB, power is required, because USB OTG port will be used to download images into Flash/SD/eMMC on board.

   In addition, 24MHz crystal is working clock for CPU, so it must be used.

Best regards,

Weidong

0 项奖励
回复

695 次查看
翔李
Contributor IV

THANKS.

I find a description about PCIE on AN4397  SATA VP VPH to be ground if not in use,so si it to be ground or NC? what about PCIE-HDMI?pastedImage_1.png

0 项奖励
回复