Can I do not supply power for PCIE-HDMI-SATA-USB if not use them?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can I do not supply power for PCIE-HDMI-SATA-USB if not use them?

748件の閲覧回数
翔李
Contributor IV

HI,

If I don't use PCIE,SATA,HDMI,USB OF IMX6Q-IMX6 DUAL-SOLO etc,is it necessary to supply the power of their VCC-IN PIN? Can I NC these following PINS?
SATA_VP_VPH,,,HDMI_VP_VPH,,,PCIE_VP_VPH_VPTX,,,USB_VBUS.

What is more,If I don't use USB,Can I do not stuff 24MHZ CRYSTAL?

pastedImage_1.png

pastedImage_2.png

pastedImage_3.png

pastedImage_4.png

0 件の賞賛
返信
2 返答(返信)

617件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,

  For PCIE,SATA & HDMI, if you don't use them, not necessary to supply them, so you can make corresponding resistors NC.

  But for USB, power is required, because USB OTG port will be used to download images into Flash/SD/eMMC on board.

   In addition, 24MHz crystal is working clock for CPU, so it must be used.

Best regards,

Weidong

0 件の賞賛
返信

617件の閲覧回数
翔李
Contributor IV

THANKS.

I find a description about PCIE on AN4397  SATA VP VPH to be ground if not in use,so si it to be ground or NC? what about PCIE-HDMI?pastedImage_1.png

0 件の賞賛
返信