Can Android BSP build with multi-thread?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can Android BSP build with multi-thread?

2,153 次查看
DeanHuang
Contributor III

Hi,

I would like to build i.MX6 Android BSP with multi-thread,

make PRODUCT-sabresd_6dq-eng- -j4 2>&1 | tee build_sabresd_6dq_android.log

but some files will not be built in out/target/product/sabresd_6dq/.

ex: system.img, recovery.img  (see out.png)

These files will be built if I do not use -jN

make PRODUCT-sabresd_6dq-eng- 2>&1 | tee build_sabresd_6dq_android.log

Does I use the wrong instruction?

标签 (2)
标记 (1)
0 项奖励
回复
2 回复数

1,879 次查看
LeonardoSandova
Specialist I

In the case you don't specify the -JN, do you see the images? any error log on the compilation?

Leo

0 项奖励
回复

1,879 次查看
DeanHuang
Contributor III

Hi Leo,

If I don't specify -jN, I can see the image under out/target/product/sabresd_6dq/.


drwxrwxr-x  8 dean dean      4096 Mar 27 14:25 ./

drwxrwxr-x  3 dean dean      4096 Mar 27 10:15 ../

-rw-rw-r--     1 dean dean        14 Mar 27 14:25 android-info.txt

-rw-r--r--      1 dean dean   4263936 Mar 27 14:25 boot.img

-rw-rw-r--     1 dean dean     15908 Mar 27 10:44 clean_steps.mk

drwxrwxr-x  4 dean dean      4096 Mar 27 11:28 data/

-rw-rw-r--     1 dean dean     48870 Mar 27 14:25 installed-files.txt

-rwxr-xr-x  1 dean dean   4093120 Mar 27 10:56 kernel*

drwxrwxr-x 14 dean dean      4096 Mar 27 14:13 obj/

-rw-rw-r--  1 dean dean       353 Mar 27 10:44 previous_build_config.mk

-rw-rw-r--  1 dean dean    167791 Mar 27 14:25 ramdisk.img

-rw-rw-r--  1 dean dean    938487 Mar 27 14:25 ramdisk-recovery.img

drwxrwxr-x  3 dean dean      4096 Mar 27 14:25 recovery/

-rw-r--r--  1 dean dean   5036032 Mar 27 14:25 recovery.img

drwxrwxr-x  8 dean dean      4096 Mar 27 10:20 root/

drwxrwxr-x  5 dean dean      4096 Mar 27 14:10 symbols/

drwxrwxr-x 11 dean dean      4096 Mar 27 13:44 system/

-rw-r--r--  1 dean dean 293601280 Mar 27 14:25 system.img

-rwxr-xr-x  1 dean dean    455936 Mar 27 10:22 u-boot-6dl.bin*

-rwxr-xr-x  1 dean dean    456240 Mar 27 10:21 u-boot-6q.bin*

-rwxr-xr-x  1 dean dean    455936 Mar 27 10:22 u-boot.bin*

-rwxr-xr-x  1 dean dean   4093184 Mar 27 10:56 uImage*

-rw-r--r--  1 dean dean 134217728 Mar 27 14:25 userdata.img

0 项奖励
回复