Camera module with parallel interface for RD-IMX6Q-SABRE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Camera module with parallel interface for RD-IMX6Q-SABRE

1,974 Views
mbogenschuetz
Contributor I

Does anyone know a matching replacement board for the parallel camera module OV05642-MRSL-A01A ?

The OV05642-MRSL-A01A is discontinued and cannot be bought anymore as far as I can see.

(see https://www.ovt.com/download/datasets/6355/2QF14%20PDN%20Notification%202013%200930.pdf )

Or is there any other suitable camera module with parallel interface available for the RD-IMX6Q-SABRE Board?

Thanks for your help

0 Kudos
Reply
3 Replies

1,897 Views
joanxie
NXP TechSupport
NXP TechSupport

currently nxp official bsp supports ov5640 and ov5642 for imx6 board, maybe you can try to use ov5640

0 Kudos
Reply

1,897 Views
mbogenschuetz
Contributor I

Hi Joan,

thanks for your reply.

Do you know if there is a suitable ov5640 board with parallel video output for the RD-IMX6Q-SABRE Board available?

The only reason why I was looking for the OV05642-MRSL-A01A is the parallel video output, as we have to use this in our setup

0 Kudos
Reply

1,897 Views
joanxie
NXP TechSupport
NXP TechSupport

ov5640 is mipi camera, current bsp for imx6q only supports ov5640 and ov5642, for new camera, you need to porting by yourself, maybe you can consider OV8820

0 Kudos
Reply