Camera Support/Use in iMXRT1064

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Camera Support/Use in iMXRT1064

1,377件の閲覧回数
jagan_k
Contributor II

Hi,
   We are currently using the iMX RT1064 in one of our projects and we are planning to use this same RT1064 for a camera related Project. But looks that RT1064 has only Parallel CSI not the serial, and we have planned to add a Bridge IC for that.
Requirement for this project  is 2MP camera(1080p) with real-time Video Streaming and Monitor.

Is it advisable to use the Same iMX RT1064 for our project or can we move to another Processor?

 

Thanks
Jagan K

0 件の賞賛
返信
1 返信

1,364件の閲覧回数
Miguel04
NXP TechSupport
NXP TechSupport

Hi @jagan_k 

The IMRT1064 could be suitable for your application, however I cannot assure you that it will have an amazing performance, I recommend you iMXRT1170 or a i.MX processors since these are better options for streaming applications.

Best Regards, Miguel.

0 件の賞賛
返信