Camera ISP Tuning Environment for iMX8M Plus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Camera ISP Tuning Environment for iMX8M Plus

Jump to solution
5,342 Views
orange8park
Contributor I

Hi,

I'm developing vision camera with iMX8M Plus.

Now I'm considering use either external ISP or integrated ISP in iMX8M Plus.

To make a decision, I need information

- Can iMX8M Plus provide tuning simulator?

- Customer can control each ISP block such as BPC - Shading - Gamma - Denoise - HDR - Demosaic?

- Image Quality Measurement

- To get these professional service, can we pay extra charge?

 

BR,

Chanyong.

0 Kudos
Reply
1 Solution
5,325 Views
khang_letruong
Senior Contributor III

Hi @orange8park ,

- Can iMX8M Plus provide tuning simulator?

ISP tuning/calibration and access to tuning/calibration tools could be done via NXP partners or as NXP partner : https://community.nxp.com/t5/i-MX-Processors/imx8mp-ISP-Calibration-Tool-XML-Generator/m-p/1438716

- Customer can control each ISP block such as BPC - Shading - Gamma - Denoise - HDR - Demosaic?

After having tuning/calibration service done for your selected sensor (output is XML file specific to that sensor), users could control above elements in the pipeline from their application via ISP APIs.

Some partners of NXP providing tuning/calibration service : Lantronix,  Innowave, Teknique (not NXP partner)

Regards,
K

View solution in original post

0 Kudos
Reply
3 Replies
5,326 Views
khang_letruong
Senior Contributor III

Hi @orange8park ,

- Can iMX8M Plus provide tuning simulator?

ISP tuning/calibration and access to tuning/calibration tools could be done via NXP partners or as NXP partner : https://community.nxp.com/t5/i-MX-Processors/imx8mp-ISP-Calibration-Tool-XML-Generator/m-p/1438716

- Customer can control each ISP block such as BPC - Shading - Gamma - Denoise - HDR - Demosaic?

After having tuning/calibration service done for your selected sensor (output is XML file specific to that sensor), users could control above elements in the pipeline from their application via ISP APIs.

Some partners of NXP providing tuning/calibration service : Lantronix,  Innowave, Teknique (not NXP partner)

Regards,
K

0 Kudos
Reply
5,313 Views
orange8park
Contributor I

Thanks for the share of the information.

It could be very helpful of my project.

 

BR,

Chanyong(orange8park)

0 Kudos
Reply
5,329 Views
joanxie
NXP TechSupport
NXP TechSupport

for tuning tools, you need contact partner to get it, more detailed information, pls contact local DFAE to get further information, and for professional service(maybe not free), pls contact from

"https://www.nxp.com/support/support/nxp-engineering-services/professional-support-for-processors-and..."

 

0 Kudos
Reply