There seems to be something wrong with the "Camera Enablement Package for NXP's i.MX 8M Plus Applications Processor (Basler)" aka CAMERA-ENABLEMENT-PACKAGE-IMX8MPLUS which got published 2021-04-27 04:57:00 as it show "null KB" and if clicked leads to a "Page Not Found" error.
This is the page where the link is shown:
And this is the Link I am talking about leading to the error:
And yes, I do have an NXP account and I am logged in. Thanks!
解決済! 解決策の投稿を見る。
OK, looks like that link now points to Basler's "Camera Enablement Package for NXP®s i.MX 8M Plus Applications Processor | GA" version 1.2.0 (actually 1.2.0.12) which already got released 2021-01-13. Very useful, thanks!
OK, looks like that link now points to Basler's "Camera Enablement Package for NXP®s i.MX 8M Plus Applications Processor | GA" version 1.2.0 (actually 1.2.0.12) which already got released 2021-01-13. Very useful, thanks!