Camera Driver Update

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Camera Driver Update

1,791 Views
Cococarbine
Contributor II

Hello,

I currently have a 8m nano evk with an OnSemi AS0260 camera connected to the Mini-SAS port using a custom connector board.  I am able to create a bootable SD card using the default evk linux (full) image provided by NXP.  I believe the next steps are to modify or add a driver for the camera.  What is the procedure, or where are the files that I need to modify to communicate with this camera?

Labels (1)
0 Kudos
Reply
1 Reply

1,782 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ed

 

for new camera may be useful to look at

i.MX Linux Reference Manual​     

i.MX Porting Guide

https://www.digi.com/resources/documentation/digidocs/embedded/dey/2.6/cc8mnano/bsp_r_camera_8m
 example for 2 lanes sensor adjusting hs-settle, clk-settle :
https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mn-evk.d...

 

Example 2 lanes MIPI-CSI.jpgExample 2 lanes MIPI-CSI.jpg

Best regards
igor

0 Kudos
Reply