CTS test "testRefreshRate" failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CTS test "testRefreshRate" failed

1,840 Views
raxesh
Contributor I

Hello,

I am running into an issue i.e. fps(frames per second) is getting reduced to almost half in case of both IPUs are in active state simultaneously.

 

Issue Description :

I am using i.mx6Dual (MCIMX6D5EYM10AC) SoC. As per our requirement we are using two displays with this SoC. 1st display is connected to LVDS0 interface and routed by IPU2(second IPU) whereas 2nd display is connected to parallel interface through THC63LVDM83E which converts 28bits of CMOS/TTL data into LVDS data stream and routed by IPU1(first IPU).

When I run cts test i.e. testRefreshRate which tests fps, I get 31 fps, hence it gets failed because required fps is 60.

As one fellow suggested in this community, By Disabling LDB support by commenting out following lines from hwc_display.cpp, I am able to get 60 fps but my 2nd display is not working that means IPU1 bocomes disabled as my 2nd display is routed through IPU1.

else {
ALOGI("fb%d is %s device", i, value);
pInfo->type = HWC_DISPLAY_LDB;
pInfo->connected = true;
}

Does one IPU clock(pixel clock) affect the another one? 

Labels (4)
0 Kudos
Reply
1 Reply

1,671 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Raxesh,

IPU1 and IPU2 need use different parent clock source, this previous post might be helpful:

https://community.nxp.com/message/838442 

Regards

0 Kudos
Reply