CTS android.holo test case not running

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CTS android.holo test case not running

2,644件の閲覧回数
jblack547
Contributor II

When we run our 4.4_r1 test this test case does not run. Also, there is another holo test, android.host.holo and it doesn't even show up in the results.

The Freescale CTS test results do not mention this test case.

Anyone else having this experience?

Test Package     Passed    Failed   Timed Out    Not Executed    Total Tests

android.holo       0               0          0                   0                        0

ラベル(1)
タグ(2)
0 件の賞賛
返信
3 返答(返信)

2,180件の閲覧回数
jblack547
Contributor II

This test is officially removed from CTS for the time being. It will be put back at a future date. I removed it from the CTS.xml file to prevent the entry from messing up our test runs. We are using proprietary hardware based on SabreSD.

0 件の賞賛
返信

2,180件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi James,

Which board are you using now?
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,180件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi James,

Does it work now?

Best Regards

Dan

0 件の賞賛
返信