CST3.4.0 with HSM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CST3.4.0 with HSM

6,511 Views
jbhaijy
Contributor III

Hi,

 

I am using latest CST-3.4.0 & I want to explore the CST-3.4.0 with third party HSM. I configured openssl.cnf as like below,

openssl_conf = openssl_init
[openssl_init]
engines = engine_section
[engine_section]
pkcs11 = pkcs11_section
[pkcs11_section]
#Path to the Compiled OpenSSL PKCS11 from OpenSC - libp11
dynamic_path = /usr/lib/x86_64-linux-gnu/engines-1.1/libpkcs11.so
MODULE_PATH = /home/jbhaijy/digicert/smtools-linux-x64/smpkcs11.so

I run the CST with -b pkcs11 option to sign the images through HSM, but I am getting below errors.

./cst --verbose -b pkcs11 -i dev_spl.csf -o dev_spl.bin
Install SRK
Install CSFK
Certificate not found.
Public key certificate is invalid in file pkcs11:model=DigiCert%20PKCS%2311;manufacturer=DigiCert;serial=SS0123456789;token=Virtual%20PKCS%2311%20Token;id=%36%34%33%39%61%63%61%32%2D%35%36%61%30%2D%34%64%64%63%2D%39%36%30%39%2D%65%62%64%39%31%63%36%33%65%33%62%39;object=imx6-hab-csf2-key-test;type=private

 

Please help me identify the problems here. 

Thanks for you support.  

 

0 Kudos
Reply
9 Replies

2,832 Views
imx8mp_developer
Contributor I

I am trying to accomplish the signature using Digicert for imx93 with AHAB.

I am able to sign both os_cntr_signed.bin and  imx-boot-imx93-var-som-aski-sd.bin-flash_singleboot_gdet but once I try to verify them using ~/cst-4.0.0/linux64/bin/ahab_image_verifier I get a incoherent result:

By doing: ahab_image_verifier os_cntr_signed.bin 0 0   I get

Signature Block:
 Version: 0
 Length: 2648 bytes
 Tag: 0x90
 Certificate Offset: 0x0
 SRK Table/Array Offset: 0x10
 SRK Table:
   Tag: 0xD7
   Length: 2112 bytes
   Version: 66
   SRK Record:
     Tag: 0xE1
     Length: 527 bytes
     Sign Algorithm: RSA       
     Hash Algorithm: SHA2_384       
     Key Size/Curve: RSA4096       
     SRK Flags: CA Flags       
     Modulus (N):
.....
Signature verification failed

While by doing: ahab_image_verifier imx-boot-imx93-var-som-aski-sd.bin-flash_singleboot_gdet 0 0    I get:

Signature Block:
 Version: 0
 Length: 400 bytes
 Tag: 0x90
 Certificate Offset: 0x0
 SRK Table/Array Offset: 0x10
 SRK Table:
   Tag: 0xD7
   Length: 308 bytes
   Version: 66
   SRK Record:
     Tag: 0xE1
     Length: 76 bytes
     Sign Algorithm: ECDSA       
     Hash Algorithm: SHA2_256       
     Key Size/Curve: PRIME256V1       
     SRK Flags: None       
     X Coordinate:  ....
     Y Coordinate:  ...

......

Signature verification successful


I used the same csf.cfg as input to cst-signer, thus same SRK Table and Digicert Token are used in cst's .csf files

does anybody have a clue?! I also posted this question in here 

0 Kudos
Reply

5,788 Views
mathiyalagan_c
Contributor I

Hi @jbhaijy  how to get latest cst with hsm, unable to find the latest. 

0 Kudos
Reply

5,779 Views
jbhaijy
Contributor III

You can download from https://www.nxp.com/search?keyword=IMX_CST_TOOL
Default this CST tool have HSM support but you need to configure your CSF to get it images signed from HSM. 

Explore the documentation in this tool for further details.

0 Kudos
Reply

6,487 Views
jbhaijy
Contributor III

@hector_delgado 

Thank for the reply. 
We want to have CST signing solution for i.MX6 & i.MX8 both. Both are custom boards. I am running Ubuntu-22.04 VM.  

0 Kudos
Reply

6,459 Views
hector_delgado
NXP TechSupport
NXP TechSupport

Hi @jbhaijy ,

Have you followed all steps from our Application Note Using Code-Signing Tool with Hardware Security Module (https://www.nxp.com/webapp/Download?colCode=AN12812&location=null)?

Even though it's an old guide, I believe it should still apply to our current CST release.

Let me know if this was of any help.

Best regards,
Hector.

0 Kudos
Reply

6,440 Views
jbhaijy
Contributor III

Hi @hector_delgado 

I followed the steps mentioned in the AN12812, Instead of SoftHSM we are using 3rd party HSM. 

What could be the possible reasons?

 

Regards,

jbhaijy

0 Kudos
Reply

6,346 Views
hector_delgado
NXP TechSupport
NXP TechSupport

Hi @jbhaijy ,

Could you try the following changes to your openssl.cnf file?

openssl_conf = openssl_def

[openssl_def]
engines = engine_section


[engine_section]
pkcs11 = pkcs11_section


[pkcs11_section]
engine_id = pkcs11
#Path to the Compiled OpenSSL PKCS11 from OpenSC - libp11
dynamic_path = /usr/lib/x86_64-linux-gnu/engines-1.1/libpkcs11.so
MODULE_PATH = /home/jbhaijy/digicert/smtools-linux-x64/smpkcs11.so
init = 0


Let me know if it solves the issue.

Best regards,
Hector.

0 Kudos
Reply

6,493 Views
hector_delgado
NXP TechSupport
NXP TechSupport

Hi @jbhaijy ,

I hope you're doing well!

What i.MX are you using? Is it a custom board or one of our EVKs? Also, what distro and version of Linux are you using in your host environment? 

Best regards,
Hector.

0 Kudos
Reply