CSI0 camera, 1280x720 How do I set it to view the full image?
CSI0 ov5642 driver is used to output camera images.
Camera output is 1280x720
When the camera is activated (./mxc_v4l2_overlay.out -iw 1280 -ih 720 -ow 1280 -ih 720)
It seems that the image is only 1/4 output.
I printed the log.
End of mxc_v4l2_s_fmt: v2f pix widthxheight 288 x 352
End of mxc_v4l2_s_fmt: crop_bounds widthxheight 640 x 480
End of mxc_v4l2_s_fmt: crop_defrect widthxheight 640 x 480
End of mxc_v4l2_s_fmt: crop_current widthxheight 640 x 480
640x480 is cropped and cropped.
1280x720 How do I set it to view the full image?
In the code mxc_v4l2_capture.c, the camera information is
"vidioc_int_g_fmt_cap (cam-> sensor, & cam_fmt);"
Get settings from cam_fmt
How can I adjust these settings?