CSI and Mipi

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CSI and Mipi

1,482 Views
jiujinhong
Contributor IV

Hi,

in another thread,

"

For iMX6DQ, there are two IPUs, so they can support up to 4 cameras at the same time. But the default BSP can only support up to two cameras at the same time.

untitled.png

The attached patch can make the BSP support up to 4 cameras based on 3.10.53 GA 1.1.0 BSP.

 

The 4 cameras can be:

- 1xCSI, 3xMIPI

- 2xCSI, 2xMIPI

- 4xMIPI

 

For 4xMIPI case, the four cameras should be combined on the single MIPI CSI2 interface, and each camera data should be transfered on a mipi virtual channel.

"

Question, can you help to give explain to "1xCSI, 3xMIPI"? How about "3xCSI, 1xMIPI"?Why 4xMIPI four cameras shoule be combined on the single MIPI CSI2 interface?

Labels (4)
0 Kudos
Reply
1 Reply

1,350 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the figure, imx6 just has two CSI ports, so the max CSI number is two, and mx6 has 4 virtual channels for mipi, should be connected max 4 mipi, so you can know the reason couldn't connect 3CSI+1MIPI, because mx6 just has one mipi/csi2 port, so 4 mipi need to combined on the single MIPI CSI2 interface

0 Kudos
Reply