CSI Statistic Data

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CSI Statistic Data

1,524 Views
fabian1993
Contributor I

Hello

I'm using the i.MX7D processor. In the reference manual I have seen that the Camera Serial Interface creates statistic data for automatic white balance and so on.

But in the driver source code I couldn't find any function which reads out this data. So my question is there any working example which reads out the statistic data?

Best regards

Fabian

Labels (2)
Tags (2)
0 Kudos
Reply
1 Reply

1,460 Views
igorpadykov
NXP Employee
NXP Employee

Hi Fabian

I am afraid such examples for sensor statistic data are not available, sorry.

In general nxp has extended support for helping with creating such drivers

NXP Professional Services | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply