CSI Statistic Data

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CSI Statistic Data

1,515件の閲覧回数
fabian1993
Contributor I

Hello

I'm using the i.MX7D processor. In the reference manual I have seen that the Camera Serial Interface creates statistic data for automatic white balance and so on.

But in the driver source code I couldn't find any function which reads out this data. So my question is there any working example which reads out the statistic data?

Best regards

Fabian

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 返信

1,451件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Fabian

I am afraid such examples for sensor statistic data are not available, sorry.

In general nxp has extended support for helping with creating such drivers

NXP Professional Services | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信