CS pin status in spi-imx.c

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CS pin status in spi-imx.c

1,455件の閲覧回数
stevegabriel123
Contributor I

I am using i.MX 6 processor.  Where can i read ecspi4 SS0  pin status in SPI-imx.c file.(value read)

ラベル(1)
0 件の賞賛
返信
1 返信

1,389件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi steve

I am afraid driver does not have such functionality, in general one can try to

use register GPIOx_PSR associated with that pad and sion bit described in

sect.36.3.2 SW Loopback through SION bit 

i.MX 6Dual/6Quad Applications Processor Reference Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信