CRUX ARMHF test1 and GCC with Graphite -blog archive

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CRUX ARMHF test1 and GCC with Graphite -blog archive

1,063 Views
acrux
Contributor I
The upcoming test1 comes with Graphite support.

root@efikamx:~# gcc -v
Using built-in specs.
COLLECT_GCC=gcc
COLLECT_LTO_WRAPPER=/usr/lib/gcc/arm-unknown-linux-gnueabihf/4.6.1/lto-wrapper
Target: arm-unknown-linux-gnueabihf
Configured with: ../gcc-4.6-20110610/configure --prefix=/usr --mandir=/usr/man
--libexecdir=/usr/lib --enable-languages=c,c++,objc --enable-threads=posix
--enable-__cxa_atexit --enable-clocale=gnu --enable-shared --with-ppl 
--enable-cloog-backend=isl --with-arch=armv7-a --with-mode=thumb
--with-float=hard --with-fpu=vfpv3-d16 --with-abi=aapcs-linux --disable-nls 
--with-x=no --with-system-zlib --build=arm-unknown-linux-gnueabihf
--with-pkgversion='CRUX ARMHF'
Thread model: posix
gcc version 4.6.1 20110610 (prerelease) (CRUX ARMHF) 
Tags (1)
0 Kudos
Reply
0 Replies