CPUINFO on MX6DL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CPUINFO on MX6DL

1,301件の閲覧回数
tony_l_cai
Contributor III

Hi,all

     I want to show the cpu frequency,but when I issue the cmd "cat proc/cpuinfo", there is no cpu frequency.And when I issued the same cmd in the another linux pc,I can see the cpu frequency. So how to show the cpu frequency on MX6DL?

3Q~

ラベル(3)
0 件の賞賛
返信
1 返信

1,206件の閲覧回数
Yuri
NXP Employee
NXP Employee

From Chapter 24 [CPU Frequency Scaling (CPUFREQ) Driver]
of “i.MX_6_Linux_Reference_Manual.pdf” :

Use the following command to view the current CPU frequency in KHz:

  $ cat /sys/devices/system/cpu/cpu0/cpufreq/cpuinfo_cur_freq


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信